FixturePortCollection Class¶
-
class
NXOpen.Routing.
FixturePortCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.FixturePort
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateFixturePort | Creates a FixturePort with a rotation vector at an absolute location. |
CreateFromAxis | Creates a fixture port based on an existing axis. |
CreateFromCsys | Creates a fixture port based on an existing Cartesian Coordinate System. |
Method Detail¶
CreateFixturePort¶
-
FixturePortCollection.
CreateFixturePort
¶ Overloaded method CreateFixturePort
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle)
CreateFixturePort(origin, alignmentVector)
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point)
CreateFixturePort(origin, alignmentVector, point)
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis)
CreateFixturePort(origin, alignmentVector, derivationObject)
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, allowMultipleConnections)
CreateFixturePort(origin, alignmentVector, allowMultipleConnections)
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point, allowMultipleConnections)
CreateFixturePort(origin, alignmentVector, point, allowMultipleConnections)
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis, allowMultipleConnections)
CreateFixturePort(origin, alignmentVector, derivationObject, allowMultipleConnections)
-------------------------------------
Creates a FixturePort with a rotation vector at an absolute location. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector at an absolute location. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with a rotation vector at a point. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- point (
NXOpen.Point
) – Fixture Port derived from this point
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector at a point. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector, point)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - point (
NXOpen.Point
) – Fixture Port derived from this point
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with a rotation vector on an axis. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- axis (
NXOpen.Axis
) – Fixture Port derived from this axis
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector on an axis. Default allows multiple connections to this port.
Signature
CreateFixturePort(origin, alignmentVector, derivationObject)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - derivationObject (
NXOpen.Axis
) – Fixture Port derived from this axis
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with a rotation vector at an absolute location
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector at an absolute location
Signature
CreateFixturePort(origin, alignmentVector, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with a rotation vector at a point
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, point, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- point (
NXOpen.Point
) – Fixture Port derived from this point - allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector at a point
Signature
CreateFixturePort(origin, alignmentVector, point, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - point (
NXOpen.Point
) – Fixture Port derived from this point - allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with a rotation vector on an axis
Signature
CreateFixturePort(origin, alignmentVector, rotationVector, rotationObject, clockAngle, axis, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - rotationVector (
NXOpen.Vector3d
) – Rotation Vector of the fixture port - rotationObject (
NXOpen.DisplayableObject
) – Rotation derivation object, may be None - clockAngle (float) – Clock angle increment in degrees for the rotation vector
- axis (
NXOpen.Axis
) – Fixture Port derived from this axis - allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Creates a FixturePort with no rotation vector on an axis
Signature
CreateFixturePort(origin, alignmentVector, derivationObject, allowMultipleConnections)
Parameters: - origin (
NXOpen.Point3d
) – Origin of the fixture port - alignmentVector (
NXOpen.Vector3d
) – Alignment vector of the fixture port - derivationObject (
NXOpen.Axis
) – Fixture Port derived from this axis - allowMultipleConnections (bool) – Does this fixture port allow multiple wires to be routed to it?
Returns: Return type: New in version NX5.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
CreateFromAxis¶
-
FixturePortCollection.
CreateFromAxis
¶ Creates a fixture port based on an existing axis.
Signature
CreateFromAxis(axis)
Parameters: axis ( NXOpen.Axis
) – The new Fixture Port will be derived from this axisReturns: Return type: NXOpen.Routing.FixturePort
New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
CreateFromCsys¶
-
FixturePortCollection.
CreateFromCsys
¶ Creates a fixture port based on an existing Cartesian Coordinate System.
The port aligns with the Z axis of the Coordinate System. The port’s rotation vector, if any, aligns with the Y direction of the Coordinate System.
Signature
CreateFromCsys(csys, createRotationVector)
Parameters: - csys (
NXOpen.CartesianCoordinateSystem
) – The new Fixture Port will be derived from this Cartesian Coordinate System - createRotationVector (
NXOpen.Routing.PortCreateRotationVector
) – Should the rotation vector be created?
Returns: Return type: New in version NX10.0.0.
License requirements: routing_base (“Routing Basic”)
- csys (