AddFontBuilder Class¶
-
class
NXOpen.Routing.
AddFontBuilder
¶ Bases:
NXOpen.Builder
Builder for creating an add font user interface dialogue
To obtain an instance of this class use
NXOpen.Routing.AddFontBuilder
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetBuilderData | Takes selected line and information on the font selected which will be used to build the font |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
SetBuilderData¶
-
AddFontBuilder.
SetBuilderData
¶ Takes selected line and information on the font selected which will be used to build the font
Signature
SetBuilderData(selLine, lineCoords, fontName, fontScale, fontLayer)
Parameters: - selLine (
NXOpen.Line
) – - lineCoords (list of float) – Line Coordinates for font element lines. formatted as x11,y11,x12,y12,x21,y21,x22,y22,x31,... where first subscript = line number; second subscript = start pt(1) or end pt(2) example: y32 = y coordinate of the third line’s end point
- fontName (str) – Font style chosen, eg “dashed” NOTE: The full Unicode character set is not supported for this parameter.
- fontScale (float) – Length dimension of font element measured along selected line; font element length = 2.0 * fontScale
- fontLayer (int) – 1,2,..255 are valid layers; -1 indicates font to be created in same layer as selLine
New in version NX8.5.0.
License requirements: routing_base (“Routing Basic”)
- selLine (
Validate¶
-
AddFontBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.