CompareRunsBuilder Class¶
-
class
NXOpen.Routing.
CompareRunsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.CompareRunsBuilder
, used to compare runs in the work part to the ones in another part, or to runs defined in xml files gathered in a folder (native mode) or on an item revision (managed mode).To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateCompareRunsBuilder
Default values.
Property Value CompareTypesEnum Xml New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CompareTypesEnum | Returns or sets the Compare type: part or xml |
FilterString | Returns or sets the filter used to limit which runs are compared among those in the folder or on the item revision |
InputPathString | Returns or sets the full path input to the compare runs algorithm. |
ReportDiscrepancies | Returns or sets the option to report discrepancies down to attribute level. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CompareRunsBuilderCompareTypes Enumeration | The Compare Type selection Enum. |
Property Detail¶
CompareTypesEnum¶
-
CompareRunsBuilder.
CompareTypesEnum
¶ Returns or sets the Compare type: part or xml
-------------------------------------
Getter Method
Signature
CompareTypesEnum()
Returns: Return type: NXOpen.Routing.CompareRunsBuilderCompareTypes
New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
CompareTypesEnum(compareTypesEnum)
Parameters: compareTypesEnum ( NXOpen.Routing.CompareRunsBuilderCompareTypes
) –New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FilterString¶
-
CompareRunsBuilder.
FilterString
¶ Returns or sets the filter used to limit which runs are compared among those in the folder or on the item revision
-------------------------------------
Getter Method
Signature
FilterString()
Returns: Return type: str New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FilterString(filterString)
Parameters: filterString (str) – New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
InputPathString¶
-
CompareRunsBuilder.
InputPathString
¶ Returns or sets the full path input to the compare runs algorithm.
Can be a folder or an item revision for xml comparisons, or a part.
-------------------------------------
Getter Method
Signature
InputPathString()
Returns: Return type: str New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
InputPathString(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ReportDiscrepancies¶
-
CompareRunsBuilder.
ReportDiscrepancies
¶ Returns or sets the option to report discrepancies down to attribute level.
-------------------------------------
Getter Method
Signature
ReportDiscrepancies()
Returns: Return type: bool New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ReportDiscrepancies(reportDiscrepancies)
Parameters: reportDiscrepancies (bool) – New in version NX9.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
CompareRunsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.