ModelTerminalsBuilder Class¶
-
class
NXOpen.Routing.
ModelTerminalsBuilder
¶ Bases:
NXOpen.Builder
The Builder to Model/UnModel the Terminals
To create a new instance of this class, use
NXOpen.Routing.RouteManager.ModelTerminalsBuilder
Default values.
Property Value CutbackOption FromCharacteristic ExtensionOption FromCharacteristic PreviewToggle 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CutbackOption | Returns or sets the cutback option |
ExtensionOption | Returns or sets the extension option |
List | Returns the List Containing the Terminals and their properties. |
MultiPort | Returns or sets the MultiPort of the selected object |
PortSelection | Returns the port selection |
PreviewToggle | Returns or sets the preview |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Model | The Model the selected Terminals |
ModelAll | The Model all the terminals |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnModel | The UnModel the selected terminals |
UnModelAll | Unmodel all of the terminals |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ModelTerminalsBuilderCutBackLocationOption Enumeration | The Enum for selecting the CutBack Option |
ModelTerminalsBuilderExtensionValueOption Enumeration | The Enum for selecting the ExtensionValue Option |
Property Detail¶
CutbackOption¶
-
ModelTerminalsBuilder.
CutbackOption
¶ Returns or sets the cutback option
-------------------------------------
Getter Method
Signature
CutbackOption()
Returns: Return type: NXOpen.Routing.ModelTerminalsBuilderCutBackLocationOption
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
CutbackOption(cutbackOption)
Parameters: cutbackOption ( NXOpen.Routing.ModelTerminalsBuilderCutBackLocationOption
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ExtensionOption¶
-
ModelTerminalsBuilder.
ExtensionOption
¶ Returns or sets the extension option
-------------------------------------
Getter Method
Signature
ExtensionOption()
Returns: Return type: NXOpen.Routing.ModelTerminalsBuilderExtensionValueOption
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
ExtensionOption(extensionOption)
Parameters: extensionOption ( NXOpen.Routing.ModelTerminalsBuilderExtensionValueOption
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
List¶
-
ModelTerminalsBuilder.
List
¶ Returns the List Containing the Terminals and their properties.
-------------------------------------
Getter Method
Signature
List()
Returns: Return type: NXOpen.TaggedObjectList
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
MultiPort¶
-
ModelTerminalsBuilder.
MultiPort
¶ Returns or sets the MultiPort of the selected object
-------------------------------------
Getter Method
Signature
MultiPort()
Returns: Routing Port Return type: NXOpen.NXObject
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
MultiPort(port)
Parameters: port ( NXOpen.NXObject
) – Routing PortNew in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
PortSelection¶
-
ModelTerminalsBuilder.
PortSelection
¶ Returns the port selection
-------------------------------------
Getter Method
Signature
PortSelection()
Returns: Return type: NXOpen.Routing.SelectPort
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
PreviewToggle¶
-
ModelTerminalsBuilder.
PreviewToggle
¶ Returns or sets the preview
-------------------------------------
Getter Method
Signature
PreviewToggle()
Returns: Return type: bool New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
PreviewToggle(preview)
Parameters: preview (bool) – New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
Model¶
-
ModelTerminalsBuilder.
Model
¶ The Model the selected Terminals
Signature
Model()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ModelAll¶
-
ModelTerminalsBuilder.
ModelAll
¶ The Model all the terminals
Signature
ModelAll()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
UnModel¶
-
ModelTerminalsBuilder.
UnModel
¶ The UnModel the selected terminals
Signature
UnModel()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
UnModelAll¶
-
ModelTerminalsBuilder.
UnModelAll
¶ Unmodel all of the terminals
Signature
UnModelAll()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
ModelTerminalsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.