StockOffsetPointBuilder Class¶
-
class
NXOpen.Routing.
StockOffsetPointBuilder
¶ Bases:
NXOpen.Builder
Applies Assemblies Constraints to a selected
NXOpen.Point
orNXOpen.Routing.ControlPoint
to mimic the update/move behavior of the input smartNXOpen.Point
.The smart point may be a Routing stock offset point (see
NXOpen.PointCollection.CreateStockOffsetPoint
) or any of the points created using theNXOpen.PointCollection
class.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateStockOffsetPointBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConstraintPoint | Returns or sets the point that defines the location of the selected point. |
PointSelection | Returns the point selection. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPointData | Gets the stock offset data from the currently selected point or routing control point. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StockOffsetPointBuilderPointType Enumeration | Point Type |
Property Detail¶
ConstraintPoint¶
-
StockOffsetPointBuilder.
ConstraintPoint
¶ Returns or sets the point that defines the location of the selected point.
On commit, this point is used for determining the set of Assemblies Constraints to apply to the selected point (or Routing control point). The input point itself is not used after the commit method.
-------------------------------------
Getter Method
Signature
ConstraintPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ConstraintPoint(point)
Parameters: point ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
PointSelection¶
-
StockOffsetPointBuilder.
PointSelection
¶ Returns the point selection.
Stores the point or Routing control point selected by the user.
-------------------------------------
Getter Method
Signature
PointSelection()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
GetPointData¶
-
StockOffsetPointBuilder.
GetPointData
¶ Gets the stock offset data from the currently selected point or routing control point.
Signature
GetPointData()
Returns: a tuple Return type: A tuple consisting of (pointType, basePoint, offsetDir, offsetExpression). pointType is a NXOpen.Routing.StockOffsetPointBuilderPointType
. Type of point currently defined. basePoint is aNXOpen.Point
. Base point for stock offset points, None for:py:class:Routing.StockOffsetPointBuilderPointType.Normal <Routing.StockOffsetPointBuilderPointType> points. offsetDir is aNXOpen.Direction
. Offset direction for stock offset points, None for:py:class:Routing.StockOffsetPointBuilderPointType.Normal <Routing.StockOffsetPointBuilderPointType> points. offsetExpression is a str. Offset expression for stock offset points, None for:py:class:Routing.StockOffsetPointBuilderPointType.Normal <Routing.StockOffsetPointBuilderPointType> points.New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Validate¶
-
StockOffsetPointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.