ICharacteristic Class

class NXOpen.Routing.ICharacteristic

Bases: NXOpen.INXObject

Interface for querying and setting characteristic (UG attribute values) on various routing objects.

These methods should be used instead of the attribute methods on the NXObject object in order to support extra functionality such as synonym characteristics available in the Routing application. .. versionadded:: NX4.0.0