EditBendAngleBuilder Class¶
-
class
NXOpen.Routing.
EditBendAngleBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateEditBendAngleBuilder
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitCurrentEdit | Commits the current edit operation. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedBendData | Returns information about the angle being changed. |
SetMoveAttachedFlag | Move all attached geometry as a rigid set. |
SetRCP | Set the Bend RCP to edit. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SwapAnchorSegment | Swap the free and anchor segments. |
UpdateAngle | Set the vector the defines the new bend angle. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CommitCurrentEdit¶
-
EditBendAngleBuilder.
CommitCurrentEdit
¶ Commits the current edit operation.
Signature
CommitCurrentEdit()
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetSelectedBendData¶
-
EditBendAngleBuilder.
GetSelectedBendData
¶ Returns information about the angle being changed.
Signature
GetSelectedBendData()
Returns: a tuple Return type: A tuple consisting of (angle, anchorSegDir, rcpPos, planeNormal). angle is a float. Teh angle between the two segments anchorSegDir is a NXOpen.Vector3d
. The anchor Segment rcpPos is aNXOpen.Point3d
. The position of the bend rcp planeNormal is aNXOpen.Vector3d
. The normal of the plane the arc lies in.New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetMoveAttachedFlag¶
-
EditBendAngleBuilder.
SetMoveAttachedFlag
¶ Move all attached geometry as a rigid set.
Signature
SetMoveAttachedFlag(moveAttached)
Parameters: moveAttached (bool) – Whether or not to move the geometry as a rigid set. New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetRCP¶
-
EditBendAngleBuilder.
SetRCP
¶ Set the Bend RCP to edit.
Signature
SetRCP(bendRcp)
Parameters: bendRcp ( NXOpen.TaggedObject
) – Bend RcpNew in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SwapAnchorSegment¶
-
EditBendAngleBuilder.
SwapAnchorSegment
¶ Swap the free and anchor segments.
Signature
SwapAnchorSegment()
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
UpdateAngle¶
-
EditBendAngleBuilder.
UpdateAngle
¶ Set the vector the defines the new bend angle.
.
Signature
UpdateAngle(angle)
Parameters: angle (float) – The new angle. New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Validate¶
-
EditBendAngleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.