RunCollection Class¶
-
class
NXOpen.Routing.
RunCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Run
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateRun | Creates a fully defined NXOpen.Routing.Run object whose From item(s), To item(s), and Member item(s) are assigned to components in the assembly. |
FindPath | Find a run path connecting all input From items to the To items. |
Method Detail¶
CreateRun¶
-
RunCollection.
CreateRun
¶ Overloaded method CreateRun
CreateRun(runId, runType, from, to, member)
CreateRun(runId, runType, attributes, fromItems, toItems, memberItems)
CreateRun(runId, runType, attributes)
-------------------------------------
Creates a fully defined
NXOpen.Routing.Run
object whose “From” item(s), “To” item(s), and “Member” item(s) are assigned to components in the assembly.Signature
CreateRun(runId, runType, from, to, member)
Parameters: - runId (str) – Unique identifier of the Run NOTE: The full Unicode character set is not supported for this parameter.
- runType (str) – Type of the Run NOTE: The full Unicode character set is not supported for this parameter.
- from (list of
NXOpen.NXObject
) – Array of “From” items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
- to (list of
NXOpen.NXObject
) – Array of “To” items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
- member (list of
NXOpen.NXObject
) – Array of “Member” items. Must beNXOpen.Assemblies.Component
,NXOpen.Routing.ISegment
or Routing.Stock
Returns: Return type: New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates a
NXOpen.Routing.Run
with items that are not assigned to components in the assembly.Signature
CreateRun(runId, runType, attributes, fromItems, toItems, memberItems)
Parameters: - runId (str) – Unique identifier of the Run NOTE: The full Unicode character set is not supported for this parameter.
- runType (str) – Type of the Run NOTE: The full Unicode character set is not supported for this parameter.
- attributes (
NXOpen.Routing.CharacteristicList
) – Run attributes - fromItems (list of
NXOpen.Routing.RunItem
) – Array of “From” items. - toItems (list of
NXOpen.Routing.RunItem
) – Array of “To” items. - memberItems (list of
NXOpen.Routing.RunItem
) – Array of “Member” items.
Returns: Return type: New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates an empty
NXOpen.Routing.Run
using just a unique Run identifier and a type.Signature
CreateRun(runId, runType, attributes)
Parameters: - runId (str) – Unique identifier of the Run NOTE: The full Unicode character set is not supported for this parameter.
- runType (str) – Type of the Run NOTE: The full Unicode character set is not supported for this parameter.
- attributes (
NXOpen.Routing.CharacteristicList
) – Run attributes
Returns: Return type: New in version NX7.5.4.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
FindPath¶
-
RunCollection.
FindPath
¶ Find a run path connecting all input From items to the To items.
Signature
FindPath(source, target)
Parameters: - source (list of
NXOpen.NXObject
) – Array of from items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
- target (list of
NXOpen.NXObject
) – Array of to items. Must beNXOpen.Routing.Port
,NXOpen.Routing.Run
orNXOpen.Routing.ControlPoint
Returns: Array of member items. Must be
NXOpen.Assemblies.Component
,NXOpen.Routing.ISegment
or Routing.Stock :rtype: list ofNXOpen.NXObject
New in version NX8.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- source (list of