NXOpen.Die Package¶
Classes¶
NXOpen.Die.AddSurfBuilder |
Represents a NXOpen.Die.AddSurfBuilder builder |
NXOpen.Die.AddendumSectionBuilder |
Represents a NXOpen.Die.AddendumSectionBuilder which is used to create or edit an addendum section. |
NXOpen.Die.AddendumSectionUserDefinedBuilder |
Represents a NXOpen.Die.AddendumSectionUserDefinedBuilder builder used to select a previously defined section or a string of objects to define the section shape. |
NXOpen.Die.CastRelief |
Represents a cast relief feature |
NXOpen.Die.CastReliefBuilder |
Represents a NXOpen.Die.CastReliefBuilder builder |
NXOpen.Die.CastReliefParentBuilder |
Represents a Die Cast Relief sub feature. |
NXOpen.Die.ClampingSlot |
Represents a clamping slot feature |
NXOpen.Die.ClampingSlotBuilder |
Represents a Clamping Slot feature builder |
NXOpen.Die.Clearance |
Represents a die design clearance feature. |
NXOpen.Die.ClearanceBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.Clearance feature. |
NXOpen.Die.CompensateRoughDataBuilder |
Represents a NXOpen.Die.CompensateRoughDataBuilder . |
NXOpen.Die.ConnectProfileParentBuilder |
Represents a Die Connecting Profile sub feature. |
NXOpen.Die.DeckParentBuilder |
Represents a Die Deck Feature sub feature. |
NXOpen.Die.DieAssistantFlangeProfile |
Represents a NXOpen.Die.DieAssistantFlangeProfile |
NXOpen.Die.DieAssistantFlangeProfileList |
Represents a list of objects. |
NXOpen.Die.DieAssistantTrimProfile |
Represents a NXOpen.Die.DieAssistantTrimProfile |
NXOpen.Die.DieAssistantTrimProfileList |
Represents a list of objects. |
NXOpen.Die.DieAttributesBuilder |
Represents a NXOpen.Die.DieAttributesBuilder . |
NXOpen.Die.DieBooleanBuilder |
Represents a NXOpen.Die.DieBooleanBuilder . |
NXOpen.Die.DieBooleanBuilderList |
Represents a list of objects. |
NXOpen.Die.DieCollection |
Represents a Die Engineering/Design feature builder. |
NXOpen.Die.DieDirectionBuilder |
Represents a NXOpen.Die.DieDirectionBuilder . |
NXOpen.Die.DieLimitsBuilder |
Limits a path to a segment of the path. |
NXOpen.Die.DieLimitsBuilderList |
Represents a list of objects. |
NXOpen.Die.DieLocationBuilder |
Represents a NXOpen.Die.DieLocationBuilder . |
NXOpen.Die.DieLocationBuilderList |
Represents a list of objects. |
NXOpen.Die.DieLocationsBuilder |
Represents a NXOpen.Die.DieLocationsBuilder . |
NXOpen.Die.DiePlaneBuilder |
Represents a NXOpen.Die.DiePlaneBuilder . |
NXOpen.Die.DieShoe |
Represents a die shoe feature |
NXOpen.Die.DieShoeBuilder |
Represents a Die Shoe feature builder. |
NXOpen.Die.DieSimCollection |
Represents a collection of Die Simulation - Press Models |
NXOpen.Die.DrawBead |
Represents a draw bead feature. |
NXOpen.Die.DrawBeadBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.DrawBead feature. |
NXOpen.Die.DrawBeadSegmentBuilder |
Segment builder for Die Engineering draw bead. |
NXOpen.Die.DrawBeadSegmentBuilderList |
Represents a list of objects. |
NXOpen.Die.DrawBeadTaperBuilder |
Taper definition for the end of the Die Engineering Draw Bead. |
NXOpen.Die.DrawDiePunchBuilder |
Represents a Draw Die Punch feature builder. |
NXOpen.Die.DrawDiePunchSectionBuilder |
Represents a Draw Die Punch Section sub feature. |
NXOpen.Die.FaceSheetBuilder |
Represents a Face Sheet feature |
NXOpen.Die.FillArea |
Represents a die design fill area feature. |
NXOpen.Die.FillAreaBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.FillArea feature. |
NXOpen.Die.FillBuilder |
Represents an Area Fill feature |
NXOpen.Die.FingerClearanceNotch |
Represents a die design finger clearance notch feature. |
NXOpen.Die.FingerClearanceNotchBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.FingerClearanceNotch feature. |
NXOpen.Die.FlangeSteelRibChildBuilder |
Represents a Die Flange Steel Rib Child sub feature. |
NXOpen.Die.FlangeSteelRibParentBuilder |
Represents a Die Flange Steel Rib Parent sub feature. |
NXOpen.Die.FlangeTaskBuilder |
Represents a Flange Task feature builder. |
NXOpen.Die.FormTaskBuilder |
Represents a Form Task feature builder. |
NXOpen.Die.HandlingCore |
Represents a die design handling core feature. |
NXOpen.Die.HandlingCoreBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.HandlingCore feature. |
NXOpen.Die.HandlingCoreChildBuilder |
Represents a Die Handling Core Child sub feature. |
NXOpen.Die.HandlingCoreParentBuilder |
Represents a Die Handling Core Parent sub feature. |
NXOpen.Die.Heelpost |
Represents a heelpost feature |
NXOpen.Die.HeelpostBuilder |
Represents a NXOpen.Die.HeelpostBuilder builder |
NXOpen.Die.HoleChildBuilder |
Represents a Die Hole Child sub feature. |
NXOpen.Die.HoleParentBuilder |
Represents a Die Hole Parent sub feature. |
NXOpen.Die.Keyway |
Represents a keyway feature |
NXOpen.Die.KeywayBuilder |
Represents a NXOpen.Die.KeywayBuilder builder |
NXOpen.Die.KeywayChildBuilder |
Represents a Die Keyway Child sub feature. |
NXOpen.Die.KeywayParentBuilder |
Represents a Die Keyway Parent sub feature. |
NXOpen.Die.LineupBuilder |
Represents a Lineup feature builder |
NXOpen.Die.MachineRelief |
Represents a die design machine relief feature. |
NXOpen.Die.MachineReliefBuilder |
Represents a builder that is used to create or edit a NXOpen.Die.MachineRelief feature. |
NXOpen.Die.OutputCurvesBuilder |
Represents an output curves feature builder. |
NXOpen.Die.PadChildBuilder |
Represents a Die Pad Child sub feature. |
NXOpen.Die.PadParentBuilder |
Represents a Die Pad Parent sub feature. |
NXOpen.Die.PierceHoleChildBuilder |
Represents a Pierce Hole Child sub feature. |
NXOpen.Die.PierceHoleParentBuilder |
Represents a Pierce Hole Parent sub feature. |
NXOpen.Die.PierceItemBuilder |
Represents a NXOpen.Die.PierceItemBuilder |
NXOpen.Die.PierceItemBuilderList |
Represents a list of objects. |
NXOpen.Die.PierceTaskBuilder |
Represents a Pierce Task feature builder |
NXOpen.Die.PointChildBuilder |
Represents a Die Point Child sub feature. |
NXOpen.Die.PointParentBuilder |
Represents a Die Point Parent sub feature. |
NXOpen.Die.PressModel |
Represents a Die Simulation - Press Model |
NXOpen.Die.PressModelRoot |
Represents a Die Simulation - Press Model Root. |
NXOpen.Die.PressureSystemChildBuilder |
Represents a Die Pressure System Child sub feature. |
NXOpen.Die.PressureSystemParentBuilder |
Represents a Die Pressure System Parent sub feature. |
NXOpen.Die.QuickBinderBuilder |
Represents a NXOpen.Die.QuickBinderBuilder builder which builds a developable binder sheet body by adding cones, cylinders, or planes to an approximated face. |
NXOpen.Die.QuickBinderWrapBuilder |
Represents a NXOpen.Die.QuickBinderWrapBuilder builder |
NXOpen.Die.RibChildBuilder |
Represents a Die Rib Child sub feature. |
NXOpen.Die.RibParentBuilder |
Represents a Die Rib Parent sub feature. |
NXOpen.Die.RotorBuilder |
Represents a CAM Rotor feature builder. |
NXOpen.Die.RotorSectionBuilder |
Represents a Rotor Section sub feature. |
NXOpen.Die.SpringbackCompensation |
Represents a springback compensation feature. |
NXOpen.Die.SpringbackCompensationBuilder |
Used to create or edit a NXOpen.Die.SpringbackCompensation feature. |
NXOpen.Die.SteelInsertBuilder |
Represents a Steel Insert feature builder. |
NXOpen.Die.SteelInsertSectionBuilder |
Represents a Steel Insert Section sub feature. |
NXOpen.Die.SteelInsertSegmentChildBuilder |
Represents a Steel Insert Segment Child sub feature. |
NXOpen.Die.SteelInsertSegmentParentBuilder |
Represents a Steel Insert Segment Parent sub feature. |
NXOpen.Die.ThroatChildBuilder |
Represents a Die Throat Child sub feature. |
NXOpen.Die.ThroatParentBuilder |
Represents a Die Throat Parent sub feature. |
NXOpen.Die.Tip |
Represents a Tip feature. |
NXOpen.Die.TrimFlangeDieAssistant |
Represents a trim/flange die assistant |
NXOpen.Die.TrimFlangeDieAssistantBuilder |
Represents a NXOpen.Die.TrimFlangeDieAssistantBuilder |
NXOpen.Die.TrimLineDevelopmentBuilder |
Represents a NXOpen.Features.TrimLineDevelopment builder |
NXOpen.Die.TrimTaskBuilder |
Represents a Trim Task feature builder. |
NXOpen.Die.UncutRegionsBuilder |
Calculates the uncut regions of a curve given a radius value for the cut tool. |
NXOpen.Die.WearPlateLocChildBuilder |
Represents a Die Wear Plate Locator sub feature. |
NXOpen.Die.WearPlateLocParentBuilder |
Represents a Die Wear Plate Locator sub feature. |
Enumerations¶
AddSurfBuilderMethods Enumeration | Settings for the type of addendum surface being created. |
AddendumSectionBuilderSectionLocationType Enumeration | The settings indicating the location of the section being created. |
AddendumSectionBuilderSectionOrientationType Enumeration | The settings to indicate the section orientation. |
AddendumSectionBuilderSectionShapeType Enumeration | The settings to indicate the section shape. |
AddendumSectionBuilderSegmentParameterType Enumeration | The settings to indicate which parameter of the segment to lock. |
AddendumSectionBuilderSegmentType Enumeration | The settings to indicate the segment type to update. |
AddendumSectionBuilderSurfaceBuildType Enumeration | The settings to indicate the surface type. |
ClampingSlotBuilderTypes Enumeration | Clamping slot types |
ClearanceBuilderClearanceGeometryTypes Enumeration | Identifies which type of input defines the clearance. |
ClearanceBuilderTypes Enumeration | Identifies which clearance type is being created in the casting. |
CompensateRoughDataBuilderApproximationType Enumeration | Settings for the amount of approximation to perform. |
CompensateRoughDataBuilderTypes Enumeration | Settings for the type of data being compensated. |
DieAssistantFlangeProfileType Enumeration | Settings for the flange type. |
DieBooleanBuilderBooleanType Enumeration | boolean type to apply to the selected solids |
DieBuildStatusOption Enumeration | Settings for the build status of the die design sub features. |
DieDirectionBuilderDirectionType Enumeration | the options available for defining the direction |
DieLocationBuilderLocationType Enumeration | the options available for defining the location |
DiePlaneBuilderPlaneType Enumeration | the options available for defining the plane |
DirectionOption Enumeration | Settings for the profile direction. |
DrawBeadBuilderFemaleDepthTypes Enumeration | Specifies how the female depth is calculated or defined. |
DrawBeadBuilderFemaleWidthTypes Enumeration | Specifies how the feamle width is calcualted or defined. |
DrawBeadBuilderMaleBeadPositionTypes Enumeration | Identifes which casting the male bead is created in. |
DrawBeadBuilderOrientSectionToDrawTypes Enumeration | Specifies if the segment height section parameter should be oriented to the draw direction or the sheet metal normal at the section location. |
DrawBeadBuilderOrientationTypes Enumeration | Identifies the orientation of the base parameters to the sheet metal. |
DrawBeadBuilderOutputTypes Enumeration | Specifies what type of output is desired for the feature creation. |
DrawBeadBuilderProjectionDirectionTypes Enumeration | Identifes how the centerline should be projected to the placement face during processing. |
DrawBeadBuilderTransitionDefinitionTypes Enumeration | Specifies how the transition area should be determined from segment to segment within a single bead. |
DrawBeadSegmentBuilderMaleBeadWidthTypes Enumeration | value for how the male width is specified. |
DrawBeadTaperBuilderTaperTypes Enumeration | Taper types to define how the slope is created for the bead end. |
FillAreaBuilderTypes Enumeration | Identifies the area of the casting the fill is targeted for. |
FillAreaBuilderUpperLimitTypes Enumeration | Specifies how the upper limit of the fill area is defined. |
FingerClearanceNotchBuilderTypes Enumeration | Specifies what type of base geometry to build the finger clearance notch from. |
FlangeTaskBuilderCamTypes Enumeration | Settings for the cam type of the flange task. |
FlangeTaskBuilderPierceTypes Enumeration | Settings for the pierce type of the flange task. |
FlangeTaskBuilderSpringbackTypes Enumeration | Settings for the springback type of the flange task. |
HandlingCoreBuilderTypes Enumeration | Identifies how the handling Core is located in space. |
HeelpostBuilderTypes Enumeration | Heelpost types |
KeywayBuilderLocationType Enumeration | Keyway location direction relative to the die centerline coordinate system |
KeywayBuilderTypes Enumeration | Keyway runoff types |
KeywayChildBuilderLocationOption Enumeration | Settings for the location of the keyway. |
KeywayChildBuilderRunoffTypeOption Enumeration | Settings for the runoff type of the keyway. |
KeywayParentBuilderRunoffTypeOption Enumeration | Settings for the runoff type of the keyway. |
MachineReliefBuilderMainProfileTypes Enumeration | Specifies that the profile is for an exterior or interior profile. |
MachineReliefBuilderTrimSheetTypes Enumeration | Specifies what the trimming surface is defined by. |
MachineReliefBuilderTypes Enumeration | Identifies the type of structure to be added, or subtracted, to the casting. |
OutputCurvesBuilderSmoothTypes Enumeration | Settings for the curve smoothing type. |
OutputCurvesBuilderTrimCurveCreateTypes Enumeration | Settings for the trim curve creation type. |
OutputCurvesBuilderTrimCurveTypes Enumeration | Settings for the trim curve type. |
OutputCurvesBuilderTrimOutputCurveTypes Enumeration | Settings for the trim curve output type. |
PadChildBuilderShapeTypeOption Enumeration | Settings for the shape type of the die pad. |
PadParentBuilderShapeTypeOption Enumeration | Settings for the shape type of the die pads. |
PierceHoleChildBuilderShapeTypeOption Enumeration | Settings for the shape type of the pierce hole. |
PierceItemBuilderHoleShapeType Enumeration | Settings for the hole shape of individual pierces. |
PierceItemBuilderSizingMethodOption Enumeration | Settings for the sizing method of individual pierces. |
PierceTaskBuilderCamTypes Enumeration | Settings for the cam type of the pierce task. |
PierceTaskBuilderCenterPointOptionTypes Enumeration | Settings for the center point output options of the pierce task. |
PierceTaskBuilderPrecisionTypes Enumeration | Settings for the precistion type of the pierce task. |
QuickBinderBuilderEditTypes Enumeration | The type of edit to be performed on the face. |
QuickBinderBuilderTypes Enumeration | The method used to approximate the product faces. |
QuickBinderWrapBuilderEditSizeType Enumeration | Settings for the edit size type. |
QuickBinderWrapBuilderTypes Enumeration | Settings for the binder wrap sheet body type. |
SpringbackCompensationBuilderDefinedByType Enumeration | The type of input data that defines the compensation. |
SpringbackCompensationBuilderDegreeType Enumeration | The polynomial degree type. |
SpringbackCompensationBuilderResultSheetType Enumeration | The type of sheet body you would like created as output. |
SteelInsertBuilderInsertTypeOption Enumeration | Settings for the insert type. |
SteelInsertSectionBuilderExtensionTypeOption Enumeration | Settings for the extension type. |
SteelInsertSegmentChildBuilderExtensionTypeOption Enumeration | Settings for the extension type. |
SteelInsertSegmentChildBuilderInsertTypeOption Enumeration | Settings for the insert type. |
SteelInsertSegmentParentBuilderExtensionTypeOption Enumeration | Settings for the extension type. |
SteelInsertSegmentParentBuilderInsertTypeOption Enumeration | Settings for the insert type. |
ThroatChildBuilderTypeOption Enumeration | Settings for the type of the throat section. |
ThroatParentBuilderTypeOption Enumeration | Settings for the type of the throat section. |
TrimLineDevelopmentBuilderConvergency Enumeration | The solver convergency level of onestep unform. |
TrimLineDevelopmentBuilderMaterialTypeName Enumeration | Indicates type of material |
TrimLineDevelopmentBuilderMeshElement Enumeration | The 2-D mesh element type of onestep unform. |
TrimLineDevelopmentBuilderOutputMethodName Enumeration | Indicates which trim curves to output |
TrimLineDevelopmentBuilderSmoothingName Enumeration | Indicates type of curve smoothing |
TrimLineDevelopmentBuilderSurface Enumeration | The surface types of onestep unform. |
TrimTaskBuilderCamTypes Enumeration | Settings for the cam type of the trim task. |
TrimTaskBuilderMatchCutTypes Enumeration | Settings for the match cut type of the trim task. |
UncutRegionsBuilderResultsType Enumeration | Indicates which side of curve to check |
WearPlateLocChildBuilderPositionType Enumeration | Settings for the positioning of the locator relative to the wear plate. |
WearPlateLocParentBuilderPositionType Enumeration | Settings for the positioning of the locator relative to the wear plate. |