UncutRegionsBuilderResultsType Enumeration¶
NXOpen.Die.UncutRegionsBuilder.ResultsType is an alias for NXOpen.Die.UncutRegionsBuilderResultsType
-
class
NXOpen.Die.
UncutRegionsBuilderResultsType
¶ Bases:
object
Indicates which side of curve to check
Enum Members
Enum Member Enum Member Description OneSide Find uncut regions on one side onlyBothSides Find uncut regions on both sides of curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-