DirectionOption Enumeration¶
-
class
NXOpen.Die.
DirectionOption
¶ Bases:
object
Settings for the profile direction.
Enum Members
Enum Member Enum Member Description FromEnd Profile direction is aligned with the first curve from the end to start.FromStart Profile direction is aligned with the first curve from the start to end.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-