DrawDiePunchSectionBuilder Class¶
-
class
NXOpen.Die.
DrawDiePunchSectionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Draw Die Punch Section sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BaseThickness | Returns the base thickness of the draw die punch casting. |
BaseWidth | Returns the base width of the draw die punch casting. |
BeltThickness | Returns the belt thickness of the draw die punch casting. |
BuildStatus | Returns the build status of the draw die punch casting. |
DeckThickness | Returns the deck thickness of the draw die punch casting. |
DesignStatus | Returns the design status of the draw die punch casting, if true the casting will be built into the model, if false it will not. |
DisplayStatus | Returns the display status of the draw die punch casting, if true input data to the draw die punch casting will be displayed, if false the input data will not be displayed. |
OffsetProfileToTop | Returns the offset profile to top distance of the draw die punch casting. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PartialRibHeight | Returns the partial rib height of the draw die punch casting. |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReliefAngle | Returns the relief angle of the draw die punch casting. |
ReliefDistance | Returns the relief distance of the draw die punch casting. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WallThickness | Returns the wall thickness of the draw die punch casting. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBaseAttributes | Gets the base faces attributes. |
GetBeltWallAttributes | Gets the belt wall faces attributes. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetFormingAttributes | Gets the forming faces attributes. |
GetObject | Returns the object currently being edited by this builder. |
GetPunchProfileAttributes | Gets the punch profile edges attributes. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBaseAttributes | Sets the base faces attributes. |
SetBaseThickness | |
SetBaseWidth | |
SetBeltThickness | |
SetBeltWallAttributes | Sets the belt wall faces attributes. |
SetDeckThickness | |
SetDesignStatus | |
SetDisplayStatus | |
SetFormingAttributes | Sets the forming faces attributes. |
SetOffsetProfileToTop | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPartialRibHeight | |
SetPunchProfileAttributes | Sets the punch profile edges attributes. |
SetReliefAngle | |
SetReliefDistance | |
SetWallThickness | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BaseThickness¶
-
DrawDiePunchSectionBuilder.
BaseThickness
¶ Returns the base thickness of the draw die punch casting.
-------------------------------------
Getter Method
Signature
BaseThickness()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BaseWidth¶
-
DrawDiePunchSectionBuilder.
BaseWidth
¶ Returns the base width of the draw die punch casting.
-------------------------------------
Getter Method
Signature
BaseWidth()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BeltThickness¶
-
DrawDiePunchSectionBuilder.
BeltThickness
¶ Returns the belt thickness of the draw die punch casting.
-------------------------------------
Getter Method
Signature
BeltThickness()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BuildStatus¶
-
DrawDiePunchSectionBuilder.
BuildStatus
¶ Returns the build status of the draw die punch casting.
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DeckThickness¶
-
DrawDiePunchSectionBuilder.
DeckThickness
¶ Returns the deck thickness of the draw die punch casting.
-------------------------------------
Getter Method
Signature
DeckThickness()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
DrawDiePunchSectionBuilder.
DesignStatus
¶ Returns the design status of the draw die punch casting, if true the casting will be built into the model, if false it will not.
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
DrawDiePunchSectionBuilder.
DisplayStatus
¶ Returns the display status of the draw die punch casting, if true input data to the draw die punch casting will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
OffsetProfileToTop¶
-
DrawDiePunchSectionBuilder.
OffsetProfileToTop
¶ Returns the offset profile to top distance of the draw die punch casting.
-------------------------------------
Getter Method
Signature
OffsetProfileToTop()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
PartialRibHeight¶
-
DrawDiePunchSectionBuilder.
PartialRibHeight
¶ Returns the partial rib height of the draw die punch casting.
-------------------------------------
Getter Method
Signature
PartialRibHeight()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ReliefAngle¶
-
DrawDiePunchSectionBuilder.
ReliefAngle
¶ Returns the relief angle of the draw die punch casting.
-------------------------------------
Getter Method
Signature
ReliefAngle()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetBaseAttributes¶
-
DrawDiePunchSectionBuilder.
GetBaseAttributes
¶ Gets the base faces attributes.
Signature
GetBaseAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of base faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetBeltWallAttributes¶
-
DrawDiePunchSectionBuilder.
GetBeltWallAttributes
¶ Gets the belt wall faces attributes.
Signature
GetBeltWallAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of belt wall faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetFormingAttributes¶
-
DrawDiePunchSectionBuilder.
GetFormingAttributes
¶ Gets the forming faces attributes.
Signature
GetFormingAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of forming faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetPunchProfileAttributes¶
-
DrawDiePunchSectionBuilder.
GetPunchProfileAttributes
¶ Gets the punch profile edges attributes.
Signature
GetPunchProfileAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value). title is a str. Title for attribute. value is a str. Value of attribute. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBaseAttributes¶
-
DrawDiePunchSectionBuilder.
SetBaseAttributes
¶ Sets the base faces attributes.
Signature
SetBaseAttributes(title, value, color)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – Color of base faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBaseThickness¶
-
DrawDiePunchSectionBuilder.
SetBaseThickness
¶ Signature
SetBaseThickness(baseThickness)
Parameters: baseThickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBaseWidth¶
-
DrawDiePunchSectionBuilder.
SetBaseWidth
¶ Signature
SetBaseWidth(baseWidth)
Parameters: baseWidth (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBeltThickness¶
-
DrawDiePunchSectionBuilder.
SetBeltThickness
¶ Signature
SetBeltThickness(beltThickness)
Parameters: beltThickness (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBeltWallAttributes¶
-
DrawDiePunchSectionBuilder.
SetBeltWallAttributes
¶ Sets the belt wall faces attributes.
Signature
SetBeltWallAttributes(title, value, color)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – Color of belt wall faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDeckThickness¶
-
DrawDiePunchSectionBuilder.
SetDeckThickness
¶ Signature
SetDeckThickness(deckThickness)
Parameters: deckThickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDesignStatus¶
-
DrawDiePunchSectionBuilder.
SetDesignStatus
¶ Signature
SetDesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDisplayStatus¶
-
DrawDiePunchSectionBuilder.
SetDisplayStatus
¶ Signature
SetDisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetFormingAttributes¶
-
DrawDiePunchSectionBuilder.
SetFormingAttributes
¶ Sets the forming faces attributes.
Signature
SetFormingAttributes(title, value, color)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – Color of forming faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetOffsetProfileToTop¶
-
DrawDiePunchSectionBuilder.
SetOffsetProfileToTop
¶ Signature
SetOffsetProfileToTop(offsetProfileToTop)
Parameters: offsetProfileToTop (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPartialRibHeight¶
-
DrawDiePunchSectionBuilder.
SetPartialRibHeight
¶ Signature
SetPartialRibHeight(partialRibHeight)
Parameters: partialRibHeight (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPunchProfileAttributes¶
-
DrawDiePunchSectionBuilder.
SetPunchProfileAttributes
¶ Sets the punch profile edges attributes.
Signature
SetPunchProfileAttributes(title, value)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetReliefAngle¶
-
DrawDiePunchSectionBuilder.
SetReliefAngle
¶ Signature
SetReliefAngle(reliefAngle)
Parameters: reliefAngle (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetReliefDistance¶
-
DrawDiePunchSectionBuilder.
SetReliefDistance
¶ Signature
SetReliefDistance(reliefDistance)
Parameters: reliefDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetWallThickness¶
-
DrawDiePunchSectionBuilder.
SetWallThickness
¶ Signature
SetWallThickness(wallThickness)
Parameters: wallThickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
DrawDiePunchSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.