DieDirectionBuilderDirectionType Enumeration¶
NXOpen.Die.DieDirectionBuilder.DirectionType is an alias for NXOpen.Die.DieDirectionBuilderDirectionType
-
class
NXOpen.Die.
DieDirectionBuilderDirectionType
¶ Bases:
object
the options available for defining the direction
Enum Members
Enum Member Enum Member Description Selection Select a coordinate system (-Z) or plane for the direction.CoordinateSystem Define a coordinate system (-Z) for the direction.Vector Define a vector for the direction.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-