SpringbackCompensationBuilderResultSheetType Enumeration¶
NXOpen.Die.SpringbackCompensationBuilder.ResultSheetType is an alias for NXOpen.Die.SpringbackCompensationBuilderResultSheetType
-
class
NXOpen.Die.
SpringbackCompensationBuilderResultSheetType
¶ Bases:
object
The type of sheet body you would like created as output.
Enum Members
Enum Member Enum Member Description Compensated Compensated sheet body.Sprung Sprung sheet body.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-