TrimTaskBuilderMatchCutTypes Enumeration¶
NXOpen.Die.TrimTaskBuilder.MatchCutTypes is an alias for NXOpen.Die.TrimTaskBuilderMatchCutTypes
-
class
NXOpen.Die.
TrimTaskBuilderMatchCutTypes
¶ Bases:
object
Settings for the match cut type of the trim task.
Enum Members
Enum Member Enum Member Description None No match cut.AtStart At start plane only.AtEnd At end plane only.AtBoth At both start and end planes.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-