AddSurfBuilderMethods Enumeration¶
NXOpen.Die.AddSurfBuilder.Methods is an alias for NXOpen.Die.AddSurfBuilderMethods
-
class
NXOpen.Die.
AddSurfBuilderMethods
¶ Bases:
object
Settings for the type of addendum surface being created.
Enum Members
Enum Member Enum Member Description Sectional Sweep section around tangency curve.CurveMesh Modeling curve mesh.ChannelTunnelCap To close an end cap.MultiFaceBlend Face blend between sets of walls.WallsOnly Produces just the walls, no blend.DiskFaceBlend Disk type face blend.SphereFaceBlend Spherical type face blend.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-