PadChildBuilderShapeTypeOption Enumeration¶
NXOpen.Die.PadChildBuilder.ShapeTypeOption is an alias for NXOpen.Die.PadChildBuilderShapeTypeOption
-
class
NXOpen.Die.
PadChildBuilderShapeTypeOption
¶ Bases:
object
Settings for the shape type of the die pad.
Enum Members
Enum Member Enum Member Description Rectangular Rectangular pad.Circular Circular pad.Curve Curve defined pad.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-