WearPlateLocChildBuilder Class¶
-
class
NXOpen.Die.
WearPlateLocChildBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Wear Plate Locator sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of wear plate and locators |
DesignStatus | Returns or sets the design status of wear plate and locators |
DisplayStatus | Returns or sets the display status of wear plate and locators |
LocatorDepth | Returns the locator depth of die wear plate and locators |
LocatorPosition | Returns or sets the locator position of die wear plate and locators |
LocatorWidth | Returns the locator width of die wear plate and locators |
Orientation | Returns or sets the orientation plane of die wear plate and locators |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Point | Returns the point location along the centerline of die wear plate and locators |
ReverseNormal | Returns or sets the reverse normal setting of die wear plate and locators |
RibSupportWidth | Returns the wear plate rib support width of die wear plate and locators |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WearPlateLength | Returns the wear plate length of die wear plate and locators |
WearPlateWidth | Returns the wear plate width of die wear plate and locators |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetPadAttributes | Gets the pad attributes, note existance of attributes depends on usage in main feature |
GetRecessAttributes | Gets the recess attributes |
GetReliefAttributes | Gets the relief attributes |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetLocatorDepth | |
SetLocatorWidth | |
SetPadAttributes | Sets the pad attributes, note existance of attributes depends on usage in main feature |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetPoint | |
SetRecessAttributes | Sets the recess attributes |
SetReliefAttributes | Sets the relief attributes |
SetRibSupportWidth | |
SetWearPlateLength | |
SetWearPlateWidth | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WearPlateLocChildBuilderPositionType Enumeration | Settings for the positioning of the locator relative to the wear plate. |
Property Detail¶
BuildStatus¶
-
WearPlateLocChildBuilder.
BuildStatus
¶ Returns the build status of wear plate and locators
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
WearPlateLocChildBuilder.
DesignStatus
¶ Returns or sets the design status of wear plate and locators
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
WearPlateLocChildBuilder.
DisplayStatus
¶ Returns or sets the display status of wear plate and locators
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LocatorDepth¶
-
WearPlateLocChildBuilder.
LocatorDepth
¶ Returns the locator depth of die wear plate and locators
-------------------------------------
Getter Method
Signature
LocatorDepth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LocatorPosition¶
-
WearPlateLocChildBuilder.
LocatorPosition
¶ Returns or sets the locator position of die wear plate and locators
-------------------------------------
Getter Method
Signature
LocatorPosition()
Returns: Return type: NXOpen.Die.WearPlateLocChildBuilderPositionType
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
LocatorPosition(position)
Parameters: position ( NXOpen.Die.WearPlateLocChildBuilderPositionType
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
LocatorWidth¶
-
WearPlateLocChildBuilder.
LocatorWidth
¶ Returns the locator width of die wear plate and locators
-------------------------------------
Getter Method
Signature
LocatorWidth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Orientation¶
-
WearPlateLocChildBuilder.
Orientation
¶ Returns or sets the orientation plane of die wear plate and locators
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Point¶
-
WearPlateLocChildBuilder.
Point
¶ Returns the point location along the centerline of die wear plate and locators
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ReverseNormal¶
-
WearPlateLocChildBuilder.
ReverseNormal
¶ Returns or sets the reverse normal setting of die wear plate and locators
-------------------------------------
Getter Method
Signature
ReverseNormal()
Returns: Return type: int New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ReverseNormal(reverseNormal)
Parameters: reverseNormal (int) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
RibSupportWidth¶
-
WearPlateLocChildBuilder.
RibSupportWidth
¶ Returns the wear plate rib support width of die wear plate and locators
-------------------------------------
Getter Method
Signature
RibSupportWidth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
WearPlateLength¶
-
WearPlateLocChildBuilder.
WearPlateLength
¶ Returns the wear plate length of die wear plate and locators
-------------------------------------
Getter Method
Signature
WearPlateLength()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
WearPlateWidth¶
-
WearPlateLocChildBuilder.
WearPlateWidth
¶ Returns the wear plate width of die wear plate and locators
-------------------------------------
Getter Method
Signature
WearPlateWidth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetPadAttributes¶
-
WearPlateLocChildBuilder.
GetPadAttributes
¶ Gets the pad attributes, note existance of attributes depends on usage in main feature
Signature
GetPadAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. title for attribute value is a str. value of attribute color is a int. color of pad faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetRecessAttributes¶
-
WearPlateLocChildBuilder.
GetRecessAttributes
¶ Gets the recess attributes
Signature
GetRecessAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. title for attribute value is a str. value of attribute color is a int. color of recess faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetReliefAttributes¶
-
WearPlateLocChildBuilder.
GetReliefAttributes
¶ Gets the relief attributes
Signature
GetReliefAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. title for attribute value is a str. value of attribute color is a int. color of relief faces New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetLocatorDepth¶
-
WearPlateLocChildBuilder.
SetLocatorDepth
¶ Signature
SetLocatorDepth(depth)
Parameters: depth (str) – Expression Value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetLocatorWidth¶
-
WearPlateLocChildBuilder.
SetLocatorWidth
¶ Signature
SetLocatorWidth(width)
Parameters: width (str) – Expression Value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPadAttributes¶
-
WearPlateLocChildBuilder.
SetPadAttributes
¶ Sets the pad attributes, note existance of attributes depends on usage in main feature
Signature
SetPadAttributes(title, value, color)
Parameters: - title (str) – title for attribute NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – value of attribute NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – color of pad faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPoint¶
-
WearPlateLocChildBuilder.
SetPoint
¶ Signature
SetPoint(pointLocation)
Parameters: pointLocation (str) – Length along centerline expression value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetRecessAttributes¶
-
WearPlateLocChildBuilder.
SetRecessAttributes
¶ Sets the recess attributes
Signature
SetRecessAttributes(title, value, color)
Parameters: - title (str) – title for attribute NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – value of attribute NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – color of recess faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetReliefAttributes¶
-
WearPlateLocChildBuilder.
SetReliefAttributes
¶ Sets the relief attributes
Signature
SetReliefAttributes(title, value, color)
Parameters: - title (str) – title for attribute NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – value of attribute NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – color of relief faces
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetRibSupportWidth¶
-
WearPlateLocChildBuilder.
SetRibSupportWidth
¶ Signature
SetRibSupportWidth(ribSupportWidth)
Parameters: ribSupportWidth (str) – Expression Value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetWearPlateLength¶
-
WearPlateLocChildBuilder.
SetWearPlateLength
¶ Signature
SetWearPlateLength(length)
Parameters: length (str) – Expression Value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetWearPlateWidth¶
-
WearPlateLocChildBuilder.
SetWearPlateWidth
¶ Signature
SetWearPlateWidth(width)
Parameters: width (str) – Expression Value NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
WearPlateLocChildBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.