CompensateRoughDataBuilderApproximationType Enumeration¶
NXOpen.Die.CompensateRoughDataBuilder.ApproximationType is an alias for NXOpen.Die.CompensateRoughDataBuilderApproximationType
-
class
NXOpen.Die.
CompensateRoughDataBuilderApproximationType
¶ Bases:
object
Settings for the amount of approximation to perform.
Enum Members
Enum Member Enum Member Description Coarse Perform a coarse approximation.Rough Perform a rough approximation.Fine Perform a fine approximation.Exact Perform no approximation.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-