DrawBeadSegmentBuilder Class¶
-
class
NXOpen.Die.
DrawBeadSegmentBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Segment builder for Die Engineering draw bead.
The segment is defined along the centerline by either a single point (and then the next segment) or 2 end points along the segment. To create a new instance of this class, use
NXOpen.Die.DrawBeadBuilder.CreateDrawBeadSegment
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
EndLocation | Returns the end location along the centerline for this segment. |
FemaleLeftRadius | Returns the expression containing the female left radius value. |
FemaleRightRadius | Returns the expression containing the female right radius value. |
Flow | Returns or sets the value identifying if the segment is of flow type (the top radius is half the width). |
MaleBeadHeight | Returns the expression containing the male bead height value. |
MaleBeadWidthType | Returns or sets the male bead width type. |
MaleLeftSheetRadius | Returns the expression containing the male sheet radius value for the Left side. |
MaleLeftTopRadius | Returns the expression containing the male top radius value for the Left side. |
MaleLeftWallAngle | Returns the expression containing the male wall angle value for the Left side. |
MaleLeftWidth | Returns the expression containing the male width value for the left side. |
MaleRightSheetRadius | Returns the expression containing the male sheet radius value for the Right side. |
MaleRightTopRadius | Returns the expression containing the male top radius value for the Right side. |
MaleRightWallAngle | Returns the expression containing the male wall angle value for the Right side. |
MaleRightWidth | Returns the expression containing the male width value for the Right side. |
MaleTransitionLength | Returns the expression containing the male transition length value. |
StartLocation | Returns the start location along the centerline for this segment. |
Symmetry | Returns or sets the value identifying that the male width is symmetrical about the location and reference direction. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawBeadSegmentBuilderMaleBeadWidthTypes Enumeration | value for how the male width is specified. |
Property Detail¶
EndLocation¶
-
DrawBeadSegmentBuilder.
EndLocation
¶ Returns the end location along the centerline for this segment.
-------------------------------------
Getter Method
Signature
EndLocation()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: None.
FemaleLeftRadius¶
-
DrawBeadSegmentBuilder.
FemaleLeftRadius
¶ Returns the expression containing the female left radius value.
-------------------------------------
Getter Method
Signature
FemaleLeftRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
FemaleRightRadius¶
-
DrawBeadSegmentBuilder.
FemaleRightRadius
¶ Returns the expression containing the female right radius value.
-------------------------------------
Getter Method
Signature
FemaleRightRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Flow¶
-
DrawBeadSegmentBuilder.
Flow
¶ Returns or sets the value identifying if the segment is of flow type (the top radius is half the width).
Only allowed if the bead is symmetric.
-------------------------------------
Getter Method
Signature
Flow()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Flow(flow)
Parameters: flow (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MaleBeadHeight¶
-
DrawBeadSegmentBuilder.
MaleBeadHeight
¶ Returns the expression containing the male bead height value.
The height is measured from the centerline to the top of the bead.
-------------------------------------
Getter Method
Signature
MaleBeadHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleBeadWidthType¶
-
DrawBeadSegmentBuilder.
MaleBeadWidthType
¶ Returns or sets the male bead width type.
-------------------------------------
Getter Method
Signature
MaleBeadWidthType()
Returns: Return type: NXOpen.Die.DrawBeadSegmentBuilderMaleBeadWidthTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaleBeadWidthType(maleBeadWidthType)
Parameters: maleBeadWidthType ( NXOpen.Die.DrawBeadSegmentBuilderMaleBeadWidthTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MaleLeftSheetRadius¶
-
DrawBeadSegmentBuilder.
MaleLeftSheetRadius
¶ Returns the expression containing the male sheet radius value for the “Left” side.
-------------------------------------
Getter Method
Signature
MaleLeftSheetRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleLeftTopRadius¶
-
DrawBeadSegmentBuilder.
MaleLeftTopRadius
¶ Returns the expression containing the male top radius value for the “Left” side.
-------------------------------------
Getter Method
Signature
MaleLeftTopRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleLeftWallAngle¶
-
DrawBeadSegmentBuilder.
MaleLeftWallAngle
¶ Returns the expression containing the male wall angle value for the “Left” side.
-------------------------------------
Getter Method
Signature
MaleLeftWallAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleLeftWidth¶
-
DrawBeadSegmentBuilder.
MaleLeftWidth
¶ Returns the expression containing the male width value for the “left” side.
-------------------------------------
Getter Method
Signature
MaleLeftWidth()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleRightSheetRadius¶
-
DrawBeadSegmentBuilder.
MaleRightSheetRadius
¶ Returns the expression containing the male sheet radius value for the “Right” side.
-------------------------------------
Getter Method
Signature
MaleRightSheetRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleRightTopRadius¶
-
DrawBeadSegmentBuilder.
MaleRightTopRadius
¶ Returns the expression containing the male top radius value for the “Right” side.
-------------------------------------
Getter Method
Signature
MaleRightTopRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleRightWallAngle¶
-
DrawBeadSegmentBuilder.
MaleRightWallAngle
¶ Returns the expression containing the male wall angle value for the “Right” side.
-------------------------------------
Getter Method
Signature
MaleRightWallAngle()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleRightWidth¶
-
DrawBeadSegmentBuilder.
MaleRightWidth
¶ Returns the expression containing the male width value for the “Right” side.
-------------------------------------
Getter Method
Signature
MaleRightWidth()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MaleTransitionLength¶
-
DrawBeadSegmentBuilder.
MaleTransitionLength
¶ Returns the expression containing the male transition length value.
The transition length is between bead segments.
-------------------------------------
Getter Method
Signature
MaleTransitionLength()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
StartLocation¶
-
DrawBeadSegmentBuilder.
StartLocation
¶ Returns the start location along the centerline for this segment.
-------------------------------------
Getter Method
Signature
StartLocation()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX7.5.0.
License requirements: None.
Symmetry¶
-
DrawBeadSegmentBuilder.
Symmetry
¶ Returns or sets the value identifying that the male width is symmetrical about the location and reference direction.
True indictaes that it is symmetrical.
-------------------------------------
Getter Method
Signature
Symmetry()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Symmetry(symmetry)
Parameters: symmetry (bool) – New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
DrawBeadSegmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.