SpringbackCompensationBuilderDegreeType Enumeration¶
NXOpen.Die.SpringbackCompensationBuilder.DegreeType is an alias for NXOpen.Die.SpringbackCompensationBuilderDegreeType
-
class
NXOpen.Die.
SpringbackCompensationBuilderDegreeType
¶ Bases:
object
The polynomial degree type.
Acceptable degrees are 2, 3, 5, and 7.
Enum Members
Enum Member Enum Member Description Two Degree is 2Three Degree is 3Five Degree is 5Seven Degree is 7-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-