HandlingCoreChildBuilder Class¶
-
class
NXOpen.Die.
HandlingCoreChildBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Handling Core Child sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of the handling core. |
Center | Returns or sets the center of the handling core. |
Clearance | Returns or sets the clearance of the handling core. |
CoreOrientation | Returns or sets the core orientation of the handling core. |
Depth | Returns or sets the depth of the handling core. |
DesignStatus | Returns or sets the design status of the handling core, if true the handling core will be built into the model, if false it will not. |
DisplayStatus | Returns or sets the display status of the handling core, if true input data to the handling core will be displayed, if false the input data will not be displayed. |
Height | Returns or sets the height of the handling core. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseOrientation | Returns or sets the value to reverse the orientation of the core plane, if true the handling core orientation normal will be reversed, if false it will not. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Width | Returns or sets the width of the handling core. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
TranslateCenter | Translates the center of the die handling core by the specified amount. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuildStatus¶
-
HandlingCoreChildBuilder.
BuildStatus
¶ Returns the build status of the handling core.
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Center¶
-
HandlingCoreChildBuilder.
Center
¶ Returns or sets the center of the handling core.
-------------------------------------
Getter Method
Signature
Center()
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Center(center)
Parameters: center ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Clearance¶
-
HandlingCoreChildBuilder.
Clearance
¶ Returns or sets the clearance of the handling core.
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Clearance(clearance)
Parameters: clearance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CoreOrientation¶
-
HandlingCoreChildBuilder.
CoreOrientation
¶ Returns or sets the core orientation of the handling core.
-------------------------------------
Getter Method
Signature
CoreOrientation()
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CoreOrientation(coreOrientation)
Parameters: coreOrientation ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Depth¶
-
HandlingCoreChildBuilder.
Depth
¶ Returns or sets the depth of the handling core.
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Depth(depth)
Parameters: depth (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
HandlingCoreChildBuilder.
DesignStatus
¶ Returns or sets the design status of the handling core, if true the handling core will be built into the model, if false it will not.
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
HandlingCoreChildBuilder.
DisplayStatus
¶ Returns or sets the display status of the handling core, if true input data to the handling core will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Height¶
-
HandlingCoreChildBuilder.
Height
¶ Returns or sets the height of the handling core.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Height(height)
Parameters: height (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ReverseOrientation¶
-
HandlingCoreChildBuilder.
ReverseOrientation
¶ Returns or sets the value to reverse the orientation of the core plane, if true the handling core orientation normal will be reversed, if false it will not.
-------------------------------------
Getter Method
Signature
ReverseOrientation()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ReverseOrientation(reverseOrientation)
Parameters: reverseOrientation (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Width¶
-
HandlingCoreChildBuilder.
Width
¶ Returns or sets the width of the handling core.
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Width(width)
Parameters: width (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
TranslateCenter¶
-
HandlingCoreChildBuilder.
TranslateCenter
¶ Translates the center of the die handling core by the specified amount.
Signature
TranslateCenter(translateDist)
Parameters: translateDist ( NXOpen.Vector3d
) – A scaled vector indicating the distance to translateNew in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
HandlingCoreChildBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.