DieLocationBuilderLocationType Enumeration¶
NXOpen.Die.DieLocationBuilder.LocationType is an alias for NXOpen.Die.DieLocationBuilderLocationType
-
class
NXOpen.Die.
DieLocationBuilderLocationType
¶ Bases:
object
the options available for defining the location
Enum Members
Enum Member Enum Member Description SelectLocation Select the point to be used.NewPoint Define the point to be used.NewCoordinateSystem Define a coordinate system to specify the location.NewVector Define a vector to specify the location.NewPlane Define a plane to specify the location.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-