DrawBeadBuilderOutputTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.OutputTypes is an alias for NXOpen.Die.DrawBeadBuilderOutputTypes
-
class
NXOpen.Die.
DrawBeadBuilderOutputTypes
¶ Bases:
object
Specifies what type of output is desired for the feature creation.
Enum Members
Enum Member Enum Member Description None Creates a small sphere on the centerline.Male Creates the male bead only.PlusFemale Creates the male and female bead.PlusSheetMetal Creates the male, female and sheet metal bead.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-