CompensateRoughDataBuilder Class¶
-
class
NXOpen.Die.
CompensateRoughDataBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Die.CompensateRoughDataBuilder
.This class is used to edit and create a Compensate Rough Curve or Compensate Rough Sheet feature.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CompensateRoughData
Default values.
Property Value AngleTolerance 0.5 Approximation Coarse DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) JoinOutputCurves 0 MaximumGap 5.0 (millimeters part), 0.2 (inches part) ModifyInputSheet 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
Approximation | Returns or sets the approximation desired. |
CurveCollector | Returns the curve collector containing the curves that will be approximated. |
DistanceTolerance | Returns or sets the distance tolerance. |
JoinOutputCurves | Returns or sets the join output curves setting, true indicates that the output curves will be joined into a single curve. |
MaximumGap | Returns or sets the maximum gap. |
ModifyInputSheet | Returns or sets the modify input sheet setting. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProjectToFaces | Returns the faces to project the output curves onto. |
SheetBodies | Returns the sheet bodies that will be approximated. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of input data being supplied. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CompensateRoughDataBuilderApproximationType Enumeration | Settings for the amount of approximation to perform. |
CompensateRoughDataBuilderTypes Enumeration | Settings for the type of data being compensated. |
Property Detail¶
AngleTolerance¶
-
CompensateRoughDataBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Approximation¶
-
CompensateRoughDataBuilder.
Approximation
¶ Returns or sets the approximation desired.
-------------------------------------
Getter Method
Signature
Approximation()
Returns: Return type: NXOpen.Die.CompensateRoughDataBuilderApproximationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Approximation(approximation)
Parameters: approximation ( NXOpen.Die.CompensateRoughDataBuilderApproximationType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
CurveCollector¶
-
CompensateRoughDataBuilder.
CurveCollector
¶ Returns the curve collector containing the curves that will be approximated.
-------------------------------------
Getter Method
Signature
CurveCollector()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
CompensateRoughDataBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
JoinOutputCurves¶
-
CompensateRoughDataBuilder.
JoinOutputCurves
¶ Returns or sets the join output curves setting, true indicates that the output curves will be joined into a single curve.
-------------------------------------
Getter Method
Signature
JoinOutputCurves()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JoinOutputCurves(joinOutputCurves)
Parameters: joinOutputCurves (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MaximumGap¶
-
CompensateRoughDataBuilder.
MaximumGap
¶ Returns or sets the maximum gap.
-------------------------------------
Getter Method
Signature
MaximumGap()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumGap(maximumGap)
Parameters: maximumGap (float) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ModifyInputSheet¶
-
CompensateRoughDataBuilder.
ModifyInputSheet
¶ Returns or sets the modify input sheet setting.
If true the input sheet will be modified, otherwise a new sheet will be created.
-------------------------------------
Getter Method
Signature
ModifyInputSheet()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModifyInputSheet(modifyInputSheet)
Parameters: modifyInputSheet (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ProjectToFaces¶
-
CompensateRoughDataBuilder.
ProjectToFaces
¶ Returns the faces to project the output curves onto.
If faces are selected then the output curves will be projected normal to these faces.
-------------------------------------
Getter Method
Signature
ProjectToFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
SheetBodies¶
-
CompensateRoughDataBuilder.
SheetBodies
¶ Returns the sheet bodies that will be approximated.
-------------------------------------
Getter Method
Signature
SheetBodies()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Type¶
-
CompensateRoughDataBuilder.
Type
¶ Returns or sets the type of input data being supplied.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Die.CompensateRoughDataBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Die.CompensateRoughDataBuilderTypes
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
CompensateRoughDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.