FillBuilder Class¶
-
class
NXOpen.Die.
FillBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents an Area Fill feature
To create a new instance of this class, use
NXOpen.Die.DieCollection.Fill
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance of the area fill |
CopyAndMirror | Returns or sets the copy and mirror setting of the area fill |
DistanceTolerance | Returns or sets the distance tolerance of the area fill |
FillForAddendum | Returns or sets the fill for addendum setting of the area fill |
MirrorPlane | Returns or sets the plane to mirror the area fill about |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointInRegion | Returns or sets the point in region of the area fill |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TippedProduct | Returns or sets the tipped product of the area fill |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetFillShape | Gets the fill shape of the area fill @return bodies |
GetObject | Returns the object currently being edited by this builder. |
GetRegionBounds | Gets the region bounds of the area fill @return profile entries |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetFillShape | Sets the fill shape of the area fill |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegionBounds | Sets the region bounds of the area fill |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
FillBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance of the area fill
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CopyAndMirror¶
-
FillBuilder.
CopyAndMirror
¶ Returns or sets the copy and mirror setting of the area fill
-------------------------------------
Getter Method
Signature
CopyAndMirror()
Returns: = true - original sheet body will be copied in its current position and a copy will also be mirrored. the two sheet bodies will be sewn together on output = false - only mirrored copy will be produced :rtype: bool
New in version NX4.0.1.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CopyAndMirror(copyAndMirror)
Parameters: copyAndMirror (bool) – = true - original sheet body will be copied in its current position and a copy will also be mirrored. the two sheet bodies will be sewn together on output = false - only mirrored copy will be produced New in version NX4.0.1.
License requirements: die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
FillBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance of the area fill
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FillForAddendum¶
-
FillBuilder.
FillForAddendum
¶ Returns or sets the fill for addendum setting of the area fill
-------------------------------------
Getter Method
Signature
FillForAddendum()
Returns: = true - area fill is for addendum and will be called DIE_ADDENDUM_FILL :rtype: bool
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FillForAddendum(fillForAddendum)
Parameters: fillForAddendum (bool) – = true - area fill is for addendum and will be called DIE_ADDENDUM_FILL New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MirrorPlane¶
-
FillBuilder.
MirrorPlane
¶ Returns or sets the plane to mirror the area fill about
-------------------------------------
Getter Method
Signature
MirrorPlane()
Returns: Return type: NXOpen.ISurface
New in version NX4.0.1.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
MirrorPlane(mirrorPlane)
Parameters: mirrorPlane ( NXOpen.ISurface
) –New in version NX4.0.1.
License requirements: die_engineering (“DIE ENGINEERING”)
PointInRegion¶
-
FillBuilder.
PointInRegion
¶ Returns or sets the point in region of the area fill
-------------------------------------
Getter Method
Signature
PointInRegion()
Returns: Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PointInRegion(pointInRegion)
Parameters: pointInRegion ( NXOpen.Point
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TippedProduct¶
-
FillBuilder.
TippedProduct
¶ Returns or sets the tipped product of the area fill
-------------------------------------
Getter Method
Signature
TippedProduct()
Returns: Return type: NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TippedProduct(tippedProduct)
Parameters: tippedProduct ( NXOpen.Features.Feature
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
GetFillShape¶
-
FillBuilder.
GetFillShape
¶ Gets the fill shape of the area fill
Signature
GetFillShape()
Returns: bodies Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetRegionBounds¶
-
FillBuilder.
GetRegionBounds
¶ Gets the region bounds of the area fill
Signature
GetRegionBounds()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. profile entries direction is aNXOpen.Die.DirectionOption
. Profile directionNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetFillShape¶
-
FillBuilder.
SetFillShape
¶ Sets the fill shape of the area fill
Signature
SetFillShape(bodies)
Parameters: bodies (list of NXOpen.Body
) – bodiesNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetRegionBounds¶
-
FillBuilder.
SetRegionBounds
¶ Sets the region bounds of the area fill
Signature
SetRegionBounds(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction - profileEntries (list of
NXOpen.IProfile
) – profile entries
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- direction (
Validate¶
-
FillBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.