Body Class¶
-
class
NXOpen.
Body
¶ Bases:
NXOpen.DisplayableObject
,NXOpen.IOrientation
,NXOpen.IBody
Represents a Body
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
Density | Returns or sets the solid density of the body. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsSheetBody | Returns true if the body is a sheet body |
IsSolidBody | Returns true if the body is a solid body |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEdges | Returns the edges in the body @return |
GetFaces | Returns the faces in the body @return |
GetFacetedBody | Returns a faceted body for a given solid body and checks whether it is out of date. |
GetFeatures | Returns the features used to construct the body @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveMergedRibImprintedEdges | Removes imprinted edges created by the merged rib rule. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
Density¶
-
Body.
Density
¶ Returns or sets the solid density of the body.
The units of the density will be in kilograms per cubic meter
-------------------------------------
Getter Method
Signature
Density()
Returns: Return type: float New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
Density(density)
Parameters: density (float) – New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsOccurrence¶
-
Body.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsSheetBody¶
-
Body.
IsSheetBody
¶ Returns true if the body is a sheet body
-------------------------------------
Getter Method
Signature
IsSheetBody()
Returns: Return type: bool New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
IsSolidBody¶
-
Body.
IsSolidBody
¶ Returns true if the body is a solid body
-------------------------------------
Getter Method
Signature
IsSolidBody()
Returns: Return type: bool New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
JournalIdentifier¶
-
Body.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Body.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Body.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Body.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Body.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
Body.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetEdges¶
-
Body.
GetEdges
¶ Returns the edges in the body
Signature
GetEdges()
Returns: Return type: list of NXOpen.Edge
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetFaces¶
-
Body.
GetFaces
¶ Returns the faces in the body
Signature
GetFaces()
Returns: Return type: list of NXOpen.Face
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetFacetedBody¶
-
Body.
GetFacetedBody
¶ Returns a faceted body for a given solid body and checks whether it is out of date.
Signature
GetFacetedBody()
Returns: a tuple Return type: A tuple consisting of (facetBody, upToDate). facetBody is a NXOpen.Facet.FacetedBody
. upToDate is a bool.New in version NX7.5.5.
License requirements: None.
GetFeatures¶
-
Body.
GetFeatures
¶ Returns the features used to construct the body
Signature
GetFeatures()
Returns: Return type: list of NXOpen.Features.Feature
New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Print¶
-
Body.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveMergedRibImprintedEdges¶
-
Body.
RemoveMergedRibImprintedEdges
¶ Removes imprinted edges created by the merged rib rule.
Signature
RemoveMergedRibImprintedEdges(originalFace, imprintedEdges)
Parameters: - originalFace (
NXOpen.Face
) – the seed face of the rule. It can be null - imprintedEdges (list of
NXOpen.Edge
) – edges.
New in version NX6.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”)
- originalFace (
SetName¶
-
Body.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.