PierceTaskBuilderCamTypes Enumeration¶
NXOpen.Die.PierceTaskBuilder.CamTypes is an alias for NXOpen.Die.PierceTaskBuilderCamTypes
-
class
NXOpen.Die.
PierceTaskBuilderCamTypes
¶ Bases:
object
Settings for the cam type of the pierce task.
Enum Members
Enum Member Enum Member Description Direct DirectAerial Aerial CamBaseMounted Base Mounted Cam-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-