KeywayBuilderTypes Enumeration¶
NXOpen.Die.KeywayBuilder.Types is an alias for NXOpen.Die.KeywayBuilderTypes
-
class
NXOpen.Die.
KeywayBuilderTypes
¶ Bases:
object
Keyway runoff types
Enum Members
Enum Member Enum Member Description Rectangular tool runoff is perpendicular to slotCircular tool runoff is created using a plunge cut at the end of the slot-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-