PierceItemBuilderHoleShapeType Enumeration¶
NXOpen.Die.PierceItemBuilder.HoleShapeType is an alias for NXOpen.Die.PierceItemBuilderHoleShapeType
-
class
NXOpen.Die.
PierceItemBuilderHoleShapeType
¶ Bases:
object
Settings for the hole shape of individual pierces.
Enum Members
Enum Member Enum Member Description Circular Circular shaped holeOblong Oblong shaped holeSquare Square shaped holeRectangular Rectangular shaped holeRoundedRectangular Rouned Rectangular shaped holeChordRectangular Chord Rectangular holeHexagonal Hexagonal shaped holeOther Not a standard shape-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-