HandlingCoreBuilder Class¶
-
class
NXOpen.Die.
HandlingCoreBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder that is used to create or edit a
NXOpen.Die.HandlingCore
feature.To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateHandlingCoreBuilder
Default values.
Property Value Clearance.Value 100 (millimeters part), 4 (inches part) Depth.Value 40 (millimeters part), 1.6 (inches part) Height.Value 100 (millimeters part), 4 (inches part) Width.Value 75 (millimeters part), 3 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
BaseOrientation | Returns the base plane of the target. |
Clearance | Returns the expression containing the value to use for the clearance offset of the core from the base plane. |
CoreOrientation | Returns the plane of the core for deriving the rectangle and the start of the core. |
Depth | Returns the expression containing the value to use for the extrusion depth when creating the core. |
DistanceTolerance | Returns or sets the distance tolerance. |
Height | Returns the expression containing the value to use for the height of the core. |
Location | Returns the center location of the handling core. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Target | Returns the target solid the handling core will be subtracted from. |
Type | Returns or sets the indicator defining how the handling core is located in space. |
Width | Returns the expression containing the value to use for the width of the core. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HandlingCoreBuilderTypes Enumeration | Identifies how the handling Core is located in space. |
Property Detail¶
AngleTolerance¶
-
HandlingCoreBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
BaseOrientation¶
-
HandlingCoreBuilder.
BaseOrientation
¶ Returns the base plane of the target.
Used for orienting the core and offset if needed.
-------------------------------------
Getter Method
Signature
BaseOrientation()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX7.5.0.
License requirements: None.
Clearance¶
-
HandlingCoreBuilder.
Clearance
¶ Returns the expression containing the value to use for the clearance offset of the core from the base plane.
Only valid when type is
Die.HandlingCoreBuilderTypes.FromBase
orDie.HandlingCoreBuilderTypes.MapFromBase
.-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
CoreOrientation¶
-
HandlingCoreBuilder.
CoreOrientation
¶ Returns the plane of the core for deriving the rectangle and the start of the core.
Only valid when type is
Die.HandlingCoreBuilderTypes.AtLocation
.-------------------------------------
Getter Method
Signature
CoreOrientation()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX7.5.0.
License requirements: None.
Depth¶
-
HandlingCoreBuilder.
Depth
¶ Returns the expression containing the value to use for the extrusion depth when creating the core.
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
HandlingCoreBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Height¶
-
HandlingCoreBuilder.
Height
¶ Returns the expression containing the value to use for the height of the core.
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Location¶
-
HandlingCoreBuilder.
Location
¶ Returns the center location of the handling core.
-------------------------------------
Getter Method
Signature
Location()
Returns: Return type: NXOpen.Die.DieLocationsBuilder
New in version NX7.5.0.
License requirements: None.
Target¶
-
HandlingCoreBuilder.
Target
¶ Returns the target solid the handling core will be subtracted from.
-------------------------------------
Getter Method
Signature
Target()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
Type¶
-
HandlingCoreBuilder.
Type
¶ Returns or sets the indicator defining how the handling core is located in space.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Die.HandlingCoreBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Die.HandlingCoreBuilderTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Width¶
-
HandlingCoreBuilder.
Width
¶ Returns the expression containing the value to use for the width of the core.
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
HandlingCoreBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.