DrawBeadTaperBuilder Class¶
-
class
NXOpen.Die.
DrawBeadTaperBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Taper definition for the end of the Die Engineering Draw Bead.
The taper can be defined at the start, end, or both ends of the draw bead and smoothly transition the bead back into the sheet body. .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
TaperPoint | Returns or sets the point used for defining the radius value of the spherical taper. |
TaperRadius | Returns the expression containing the radius value for a spherical taper. |
TaperType | Returns or sets the method to apply for defining the taper. |
TaperWashoutHeight | Returns the expression containing the height value for a washout taper. |
TaperWashoutLength | Returns the expression containing the length value for a washout taper. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawBeadTaperBuilderTaperTypes Enumeration | Taper types to define how the slope is created for the bead end. |
Property Detail¶
TaperPoint¶
-
DrawBeadTaperBuilder.
TaperPoint
¶ Returns or sets the point used for defining the radius value of the spherical taper.
-------------------------------------
Getter Method
Signature
TaperPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaperPoint(taperPoint)
Parameters: taperPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TaperRadius¶
-
DrawBeadTaperBuilder.
TaperRadius
¶ Returns the expression containing the radius value for a spherical taper.
-------------------------------------
Getter Method
Signature
TaperRadius()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TaperType¶
-
DrawBeadTaperBuilder.
TaperType
¶ Returns or sets the method to apply for defining the taper.
-------------------------------------
Getter Method
Signature
TaperType()
Returns: Return type: NXOpen.Die.DrawBeadTaperBuilderTaperTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaperType(taperType)
Parameters: taperType ( NXOpen.Die.DrawBeadTaperBuilderTaperTypes
) –New in version NX7.5.0.
License requirements: die_engineering (“DIE ENGINEERING”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
TaperWashoutHeight¶
-
DrawBeadTaperBuilder.
TaperWashoutHeight
¶ Returns the expression containing the height value for a washout taper.
-------------------------------------
Getter Method
Signature
TaperWashoutHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TaperWashoutLength¶
-
DrawBeadTaperBuilder.
TaperWashoutLength
¶ Returns the expression containing the length value for a washout taper.
-------------------------------------
Getter Method
Signature
TaperWashoutLength()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
DrawBeadTaperBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.