PressModel Class¶
-
class
NXOpen.Die.
PressModel
¶ Bases:
NXOpen.TransientObject
Represents a Die Simulation - Press Model
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetNumOperations | Get number of operations @return |
SetOperationCushionSettings | Set operation cushion values |
SetOperationSlideHeight | Set operation slide height |
SetOperationTransportCurveSet | Tell the press model which transport curve set to use in the given operation |
SetOperationUserTransportCurves | Set values of the User Defined transport curve set, for given operation |
Method Detail¶
Dispose¶
-
PressModel.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetNumOperations¶
-
PressModel.
GetNumOperations
¶ Get number of operations
Signature
GetNumOperations()
Returns: Return type: int New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
SetOperationCushionSettings¶
-
PressModel.
SetOperationCushionSettings
¶ Set operation cushion values
Signature
SetOperationCushionSettings(operation, liftStartAngle, liftStopAngle, liftToDist, lockAtDist)
Parameters: - operation (int) – Operation of the cushion
- liftStartAngle (float) – Lift start angle
- liftStopAngle (float) – Lift stop angle
- liftToDist (float) – Distance to lift to
- lockAtDist (float) – Distance where lock happens
New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
SetOperationSlideHeight¶
-
PressModel.
SetOperationSlideHeight
¶ Set operation slide height
Signature
SetOperationSlideHeight(operation, slideHeight)
Parameters: - operation (int) – Operation of the slide
- slideHeight (float) – Slide height
New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
SetOperationTransportCurveSet¶
-
PressModel.
SetOperationTransportCurveSet
¶ Tell the press model which transport curve set to use in the given operation
Signature
SetOperationTransportCurveSet(operation, curveSet)
Parameters: - operation (int) – Operation of the transport devices
- curveSet (int) – Index of the curve set
New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
SetOperationUserTransportCurves¶
-
PressModel.
SetOperationUserTransportCurves
¶ Set values of the User Defined transport curve set, for given operation
Signature
SetOperationUserTransportCurves(operation, vals)
Parameters: - operation (int) – Operation of the transport devices
- vals (list of float) – The curve set values
New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)