ThroatParentBuilder Class¶
-
class
NXOpen.Die.
ThroatParentBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Throat Parent sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of the throat sections. |
DesignStatus | Returns or sets the design status of the throat sections, if true the throat sections will be built into the model, if false they will not. |
DisplayStatus | Returns or sets the display status of the throat sections, if true input data to the throat sections will be displayed, if false the input data will not be displayed. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Radius | Returns or sets the radius to be applied at the back of the throat, top and bottom |
Step | Returns or sets the step to be applied at the end of the tangential extension of the flange |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of throat sections. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateChild | Creates a child throat section. |
DeleteChild | Deletes a child throat section. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCavityAttributes | Gets the cavity attributes, note existance of attributes depends on usage in main feature. |
GetChildren | Outputs the child throat sections. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetExtensionAttributes | Gets the extension attributes, note existance of attributes depends on usage in main feature. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetCavityAttributes | Sets the cavity attributes, note existance of attributes depends on usage in main feature. |
SetExtensionAttributes | Sets the extension attributes, note existance of attributes depends on usage in main feature. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ThroatParentBuilderTypeOption Enumeration | Settings for the type of the throat section. |
Property Detail¶
BuildStatus¶
-
ThroatParentBuilder.
BuildStatus
¶ Returns the build status of the throat sections.
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
ThroatParentBuilder.
DesignStatus
¶ Returns or sets the design status of the throat sections, if true the throat sections will be built into the model, if false they will not.
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
ThroatParentBuilder.
DisplayStatus
¶ Returns or sets the display status of the throat sections, if true input data to the throat sections will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Radius¶
-
ThroatParentBuilder.
Radius
¶ Returns or sets the radius to be applied at the back of the throat, top and bottom
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Radius(radius)
Parameters: radius (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Step¶
-
ThroatParentBuilder.
Step
¶ Returns or sets the step to be applied at the end of the tangential extension of the flange
-------------------------------------
Getter Method
Signature
Step()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Step(step)
Parameters: step (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Type¶
-
ThroatParentBuilder.
Type
¶ Returns or sets the type of throat sections.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Die.ThroatParentBuilderTypeOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Die.ThroatParentBuilderTypeOption
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
CreateChild¶
-
ThroatParentBuilder.
CreateChild
¶ Creates a child throat section.
Signature
CreateChild()
Returns: Return type: NXOpen.Die.ThroatChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DeleteChild¶
-
ThroatParentBuilder.
DeleteChild
¶ Deletes a child throat section.
Signature
DeleteChild(diethroatchild)
Parameters: diethroatchild ( NXOpen.Die.ThroatChildBuilder
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetCavityAttributes¶
-
ThroatParentBuilder.
GetCavityAttributes
¶ Gets the cavity attributes, note existance of attributes depends on usage in main feature.
Signature
GetCavityAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of cavity faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetChildren¶
-
ThroatParentBuilder.
GetChildren
¶ Outputs the child throat sections.
Signature
GetChildren()
Returns: The child throat sections. Return type: list of NXOpen.Die.ThroatChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetExtensionAttributes¶
-
ThroatParentBuilder.
GetExtensionAttributes
¶ Gets the extension attributes, note existance of attributes depends on usage in main feature.
Signature
GetExtensionAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color). title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of extension faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetCavityAttributes¶
-
ThroatParentBuilder.
SetCavityAttributes
¶ Sets the cavity attributes, note existance of attributes depends on usage in main feature.
Signature
SetCavityAttributes(title, value, color)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – Color of cavity faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetExtensionAttributes¶
-
ThroatParentBuilder.
SetExtensionAttributes
¶ Sets the extension attributes, note existance of attributes depends on usage in main feature.
Signature
SetExtensionAttributes(title, value, color)
Parameters: - title (str) – Title for attribute. NOTE: The full Unicode character set is not supported for this parameter.
- value (str) – Value of attribute. NOTE: The full Unicode character set is not supported for this parameter.
- color (int) – Color of extension faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
ThroatParentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.