DieShoeBuilder Class¶
-
class
NXOpen.Die.
DieShoeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Shoe feature builder.
To create a new instance of this class, use
NXOpen.Die.DieCollection.DieShoe
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
BaseAttributes | Returns the base attributes |
BaseFlangeSection | Returns the base flange section |
BaseOrientation | Returns the base orientation |
CenterlineSlotAttributes | Returns the centerline slot attributes |
CenterlineSlotCreate | Returns or sets the toggle to create the centerline slot |
CenterlineSlotDepth | Returns the centerline slot depth |
CenterlineSlotDirection | Returns the centerline slot direction |
CenterlineSlotWidth | Returns the centerline slot width |
DeckCutoutsSection | Returns the cutout sections in the main deck |
DeckThickness | Returns the deck thickness |
DieBooleansList | Returns the die boolean solids list |
DistanceTolerance | Returns or sets the distance tolerance |
FlangeThickness | Returns the flange thickness |
MainDeckAttributes | Returns the main deck attributes |
MainDeckOffset | Returns the offset for the main deck either measured from the main deck specification or the base plane |
MainDeckPlane | Returns the main deck plane |
MainDeckSection | Returns the main deck section |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WallThickness | Returns the wall thickness |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
DieShoeBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
BaseAttributes¶
-
DieShoeBuilder.
BaseAttributes
¶ Returns the base attributes
-------------------------------------
Getter Method
Signature
BaseAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
BaseFlangeSection¶
-
DieShoeBuilder.
BaseFlangeSection
¶ Returns the base flange section
-------------------------------------
Getter Method
Signature
BaseFlangeSection()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
BaseOrientation¶
-
DieShoeBuilder.
BaseOrientation
¶ Returns the base orientation
-------------------------------------
Getter Method
Signature
BaseOrientation()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX6.0.0.
License requirements: None.
CenterlineSlotAttributes¶
-
DieShoeBuilder.
CenterlineSlotAttributes
¶ Returns the centerline slot attributes
-------------------------------------
Getter Method
Signature
CenterlineSlotAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
CenterlineSlotCreate¶
-
DieShoeBuilder.
CenterlineSlotCreate
¶ Returns or sets the toggle to create the centerline slot
-------------------------------------
Getter Method
Signature
CenterlineSlotCreate()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterlineSlotCreate(centerlineSlotCreate)
Parameters: centerlineSlotCreate (bool) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
CenterlineSlotDepth¶
-
DieShoeBuilder.
CenterlineSlotDepth
¶ Returns the centerline slot depth
-------------------------------------
Getter Method
Signature
CenterlineSlotDepth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
CenterlineSlotDirection¶
-
DieShoeBuilder.
CenterlineSlotDirection
¶ Returns the centerline slot direction
-------------------------------------
Getter Method
Signature
CenterlineSlotDirection()
Returns: Return type: NXOpen.Die.DieDirectionBuilder
New in version NX6.0.0.
License requirements: None.
CenterlineSlotWidth¶
-
DieShoeBuilder.
CenterlineSlotWidth
¶ Returns the centerline slot width
-------------------------------------
Getter Method
Signature
CenterlineSlotWidth()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DeckCutoutsSection¶
-
DieShoeBuilder.
DeckCutoutsSection
¶ Returns the cutout sections in the main deck
-------------------------------------
Getter Method
Signature
DeckCutoutsSection()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
DeckThickness¶
-
DieShoeBuilder.
DeckThickness
¶ Returns the deck thickness
-------------------------------------
Getter Method
Signature
DeckThickness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DieBooleansList¶
-
DieShoeBuilder.
DieBooleansList
¶ Returns the die boolean solids list
-------------------------------------
Getter Method
Signature
DieBooleansList()
Returns: Return type: NXOpen.Die.DieBooleanBuilderList
New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
DieShoeBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeThickness¶
-
DieShoeBuilder.
FlangeThickness
¶ Returns the flange thickness
-------------------------------------
Getter Method
Signature
FlangeThickness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
MainDeckAttributes¶
-
DieShoeBuilder.
MainDeckAttributes
¶ Returns the main deck attributes
-------------------------------------
Getter Method
Signature
MainDeckAttributes()
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
MainDeckOffset¶
-
DieShoeBuilder.
MainDeckOffset
¶ Returns the offset for the main deck either measured from the main deck specification or the base plane
-------------------------------------
Getter Method
Signature
MainDeckOffset()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
MainDeckPlane¶
-
DieShoeBuilder.
MainDeckPlane
¶ Returns the main deck plane
-------------------------------------
Getter Method
Signature
MainDeckPlane()
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX6.0.0.
License requirements: None.
MainDeckSection¶
-
DieShoeBuilder.
MainDeckSection
¶ Returns the main deck section
-------------------------------------
Getter Method
Signature
MainDeckSection()
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
WallThickness¶
-
DieShoeBuilder.
WallThickness
¶ Returns the wall thickness
-------------------------------------
Getter Method
Signature
WallThickness()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DieShoeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.