PierceTaskBuilderCenterPointOptionTypes Enumeration¶
NXOpen.Die.PierceTaskBuilder.CenterPointOptionTypes is an alias for NXOpen.Die.PierceTaskBuilderCenterPointOptionTypes
-
class
NXOpen.Die.
PierceTaskBuilderCenterPointOptionTypes
¶ Bases:
object
Settings for the center point output options of the pierce task.
Enum Members
Enum Member Enum Member Description None No center points outputDie Center points output in die positionProduct Center points output in product positionBoth Center points output in both die and product position-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-