FillAreaBuilderTypes Enumeration¶
NXOpen.Die.FillAreaBuilder.Types is an alias for NXOpen.Die.FillAreaBuilderTypes
-
class
NXOpen.Die.
FillAreaBuilderTypes
¶ Bases:
object
Identifies the area of the casting the fill is targeted for.
Enum Members
Enum Member Enum Member Description BaseFlange Fill area is in the base flange area.ProductContact Fill area is in the upper deck where relief for the product has been added.ScrapArea Remove the volume instead of filling. Targeted for the outer trim line area.UserDefined The user must defined all the constraints for the area (inputs from the target are ignored).-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-