FlangeTaskBuilder Class¶
-
class
NXOpen.Die.
FlangeTaskBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Flange Task feature builder.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance of the flange task |
CamDirection | Returns or sets the cam direction of the flange task |
CamType | Returns or sets the cam type of the flange task |
DisplayRotatedItems | Returns or sets the display rotated items setting of the flange task. |
DistanceTolerance | Returns or sets the distance tolerance of the flange task |
FinishOperation | Returns or sets the finish operation of the flange task |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PierceAndExtrude | Returns or sets the pierce and extrude setting of the flange task. |
PierceType | Returns or sets the pierce type of the flange task |
PointInRegion | Returns or sets the keep point in the region of the flange task |
SpringbackAngle | Returns or sets the springback angle of the flange task |
SpringbackType | Returns or sets the springback type of the flange task |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TippedProduct | Returns or sets the tipped product of the flange task |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAssociativeObjects | Gets the associative objects of the flange task @return |
GetCameraLayerAndXmlp | Gets the camera layer settings and xmlp data @return 1 layer setting string for each camera object. |
GetCameraNames | Gets the names of the camera @return each string contains the name of a camera object |
GetCameraViews | Gets the camera views of the flange task @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Gets the detailed description of the flange task @return detail strings |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetRegionBounds | Gets the region bounds of the flange task @return Profile entries that make up the boundary of the flange task |
GetShapeDetail | Gets the shape detail of the flange task for profiles @return Profile entries |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetAssociativeObjects | Sets the associative objects of the flange task |
SetCameraLayerAndXmlp | Sets the camera layer settings and xmlp data |
SetCameraNames | Sets the names of the camera |
SetCameraViews | Sets the camera views of the flange task |
SetDetails | Sets the detailed description of the flange task |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegionBounds | Sets the region bounds of the flange task |
SetShapeDetail | Sets the shape detail of the flange task for profiles |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FlangeTaskBuilderCamTypes Enumeration | Settings for the cam type of the flange task. |
FlangeTaskBuilderPierceTypes Enumeration | Settings for the pierce type of the flange task. |
FlangeTaskBuilderSpringbackTypes Enumeration | Settings for the springback type of the flange task. |
Property Detail¶
AngleTolerance¶
-
FlangeTaskBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance of the flange task
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamDirection¶
-
FlangeTaskBuilder.
CamDirection
¶ Returns or sets the cam direction of the flange task
-------------------------------------
Getter Method
Signature
CamDirection()
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamDirection(camDirection)
Parameters: camDirection ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamType¶
-
FlangeTaskBuilder.
CamType
¶ Returns or sets the cam type of the flange task
-------------------------------------
Getter Method
Signature
CamType()
Returns: Return type: NXOpen.Die.FlangeTaskBuilderCamTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamType(camType)
Parameters: camType ( NXOpen.Die.FlangeTaskBuilderCamTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DisplayRotatedItems¶
-
FlangeTaskBuilder.
DisplayRotatedItems
¶ Returns or sets the display rotated items setting of the flange task.
True indicates that the reference point and cam direction objects should be created and displayed in the die face feature.
-------------------------------------
Getter Method
Signature
DisplayRotatedItems()
Returns: Return type: bool New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DisplayRotatedItems(displaySetting)
Parameters: displaySetting (bool) – New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
FlangeTaskBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance of the flange task
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FinishOperation¶
-
FlangeTaskBuilder.
FinishOperation
¶ Returns or sets the finish operation of the flange task
-------------------------------------
Getter Method
Signature
FinishOperation()
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FinishOperation(finishOperation)
Parameters: finishOperation (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PierceAndExtrude¶
-
FlangeTaskBuilder.
PierceAndExtrude
¶ Returns or sets the pierce and extrude setting of the flange task.
True indicates that the flange task is a pierce and extrude type.
-------------------------------------
Getter Method
Signature
PierceAndExtrude()
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PierceAndExtrude(pierceAndExtrude)
Parameters: pierceAndExtrude (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PierceType¶
-
FlangeTaskBuilder.
PierceType
¶ Returns or sets the pierce type of the flange task
-------------------------------------
Getter Method
Signature
PierceType()
Returns: Return type: NXOpen.Die.FlangeTaskBuilderPierceTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PierceType(pierceType)
Parameters: pierceType ( NXOpen.Die.FlangeTaskBuilderPierceTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PointInRegion¶
-
FlangeTaskBuilder.
PointInRegion
¶ Returns or sets the keep point in the region of the flange task
-------------------------------------
Getter Method
Signature
PointInRegion()
Returns: Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PointInRegion(pointInRegion)
Parameters: pointInRegion ( NXOpen.Point
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SpringbackAngle¶
-
FlangeTaskBuilder.
SpringbackAngle
¶ Returns or sets the springback angle of the flange task
-------------------------------------
Getter Method
Signature
SpringbackAngle()
Returns: expression string Return type: str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
SpringbackAngle(springbackAngle)
Parameters: springbackAngle (str) – expression string New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SpringbackType¶
-
FlangeTaskBuilder.
SpringbackType
¶ Returns or sets the springback type of the flange task
-------------------------------------
Getter Method
Signature
SpringbackType()
Returns: Return type: NXOpen.Die.FlangeTaskBuilderSpringbackTypes
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
SpringbackType(springbackType)
Parameters: springbackType ( NXOpen.Die.FlangeTaskBuilderSpringbackTypes
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TippedProduct¶
-
FlangeTaskBuilder.
TippedProduct
¶ Returns or sets the tipped product of the flange task
-------------------------------------
Getter Method
Signature
TippedProduct()
Returns: The tip of the operation where the flange task resides. :rtype:
NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TippedProduct(tippedProduct)
Parameters: tippedProduct ( NXOpen.Features.Feature
) – The tip of the operation where the flange task resides.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
GetAssociativeObjects¶
-
FlangeTaskBuilder.
GetAssociativeObjects
¶ Gets the associative objects of the flange task
Signature
GetAssociativeObjects()
Returns: Return type: list of NXOpen.DisplayableObject
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraLayerAndXmlp¶
-
FlangeTaskBuilder.
GetCameraLayerAndXmlp
¶ Gets the camera layer settings and xmlp data
Signature
GetCameraLayerAndXmlp()
Returns: a tuple Return type: A tuple consisting of (layerSettings, xmlpData). layerSettings is a list of str. 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on. xmlpData is a list of str. xmlp data New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraNames¶
-
FlangeTaskBuilder.
GetCameraNames
¶ Gets the names of the camera
Signature
GetCameraNames()
Returns: each string contains the name of a camera object Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetCameraViews¶
-
FlangeTaskBuilder.
GetCameraViews
¶ Gets the camera views of the flange task
Signature
GetCameraViews()
Returns: Return type: list of NXOpen.View
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetDetails¶
-
FlangeTaskBuilder.
GetDetails
¶ Gets the detailed description of the flange task
Signature
GetDetails()
Returns: detail strings Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetRegionBounds¶
-
FlangeTaskBuilder.
GetRegionBounds
¶ Gets the region bounds of the flange task
Signature
GetRegionBounds()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. Profile entries that make up the boundary of the flange task direction is aNXOpen.Die.DirectionOption
. Profile directionNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetShapeDetail¶
-
FlangeTaskBuilder.
GetShapeDetail
¶ Gets the shape detail of the form task for bodies
Signature
GetShapeDetail()
Returns: bodies Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetAssociativeObjects¶
-
FlangeTaskBuilder.
SetAssociativeObjects
¶ Sets the associative objects of the flange task
Signature
SetAssociativeObjects(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraLayerAndXmlp¶
-
FlangeTaskBuilder.
SetCameraLayerAndXmlp
¶ Sets the camera layer settings and xmlp data
Signature
SetCameraLayerAndXmlp(layerSettings, xmlpData)
Parameters: - layerSettings (list of str) – 1 layer setting string for each camera object. the string needs to be 256 characters long (one for each user layer) with either 0 for off or 1 for on. NOTE: The full Unicode character set is not supported for this parameter.
- xmlpData (list of str) – xmlp data
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraNames¶
-
FlangeTaskBuilder.
SetCameraNames
¶ Sets the names of the camera
Signature
SetCameraNames(strings)
Parameters: strings (list of str) – each string contains the name of a camera object NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetCameraViews¶
-
FlangeTaskBuilder.
SetCameraViews
¶ Sets the camera views of the flange task
Signature
SetCameraViews(objects)
Parameters: objects (list of NXOpen.View
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetDetails¶
-
FlangeTaskBuilder.
SetDetails
¶ Sets the detailed description of the flange task
Signature
SetDetails(strings)
Parameters: strings (list of str) – detail strings NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetRegionBounds¶
-
FlangeTaskBuilder.
SetRegionBounds
¶ Sets the region bounds of the flange task
Signature
SetRegionBounds(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction - profileEntries (list of
NXOpen.IProfile
) – Profile entries that make up the boundary of the flange task
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- direction (
SetShapeDetail¶
-
FlangeTaskBuilder.
SetShapeDetail
¶ Overloaded method SetShapeDetail
SetShapeDetail(direction, profileEntries)
SetShapeDetail(bodies)
-------------------------------------
Sets the shape detail of the flange task for profiles
Signature
SetShapeDetail(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction - profileEntries (list of
NXOpen.IProfile
) – Profile entries
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Sets the shape detail of the form task for bodies
Signature
SetShapeDetail(bodies)
Parameters: bodies (list of NXOpen.Body
) – bodiesNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Validate¶
-
FlangeTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.