DAOConstraint Class |
Represents a NXOpen.CAE.Optimization.DAOConstraint . |
DAOConstraintBuilder Class |
Represents a NXOpen.CAE.Optimization.DAOConstraintBuilder . |
DAOConstraintCollection Class |
Represents the collection of optimization solution design constraint |
DAODesignVariable Class |
Represents a NXOpen.CAE.Optimization.DAODesignVariable . |
DAODesignVariableBuilder Class |
Represents a NXOpen.CAE.Optimization.DAODesignVariableBuilder . |
DAODesignVariableCollection Class |
Represents the collection of optimization solution design variable |
DAOObjective Class |
Represents a NXOpen.CAE.Optimization.DAOObjective . |
DAOOptimizationManager Class |
Represents the Design and Analysis optimization manager that contains all optimization objects. |
DAOSolution Class |
Represents a NXOpen.CAE.Optimization.DAOSolution . |
DAOSolutionBuilder Class |
Represents a NXOpen.CAE.Optimization.DAOSolutionBuilder . |
DAOSolutionCollection Class |
Represents the collection of optimization solution |
DAOStopCondition Class |
Represents a NXOpen.CAE.Optimization.DAOStopCondition . |
NameDescription Class |
|
TBSBaseDesignVariableBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSDesignVariable |
TBSCastCondition Class |
Represents the manufacturing restrictions of NXOpen.CAE.Optimization.TBSTopologyRestrictArea |
TBSCheckDOF Class |
Represents the restriction of dispacement in the coordinate direction of the referenced coordinate system |
TBSConstraint Class |
Represents the design constraint, which is defined with NXOpen.CAE.Optimization.TBSDesignVariable |
TBSConstraintBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSConstraint |
TBSConstraintCollection Class |
Represents a collection of NXOpen.CAE.Optimization.TBSConstraint |
TBSDesignArea Class |
Represents the design area |
TBSDesignResponse Class |
Represents the design response referenced by NXOpen.CAE.Optimization.TBSConstraint and NXOpen.CAE.Optimization.TBSObjectives |
TBSDesignResponseBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSDesignResponse |
TBSDesignVariable Class |
Represents the design variable referenced by NXOpen.CAE.Optimization.TBSConstraint and NXOpen.CAE.Optimization.TBSObjectives |
TBSDesignVariableBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSDesignVariable |
TBSDesignVariableCollection Class |
Represents a collection of CAE.Optimization.TBSDesignVariable |
TBSEigenvalueOptimizationParameters Class |
Represents the parameters to control an eigenvalue optimization |
TBSGroupDefinition Class |
Represents a group of nodes or elements |
TBSIOptimizationTest Class |
Represents an interface to perform optimization test |
TBSLoadCase Class |
Represents the load case |
TBSLoadCaseManager Class |
Managers load cases |
TBSMeshSmooth Class |
Represents the mesh smooth |
TBSObjectives Class |
Represents the objective functions of an optimization |
TBSOptimizationManager Class |
Represents the optimization manager to contain the optimization solutions and take charge of creating optimization objects |
TBSOptimizationParameters Class |
Represents the parameters to control an optimization |
TBSOptimizationSolution Class |
Represents the solution to contain optimization setting |
TBSOptimizationSolutionBuilder Class |
Represents the abstract builder of NXOpen.CAE.Optimization.TBSOptimizationSolution . |
TBSOptimizationSolutionCollection Class |
Represents a collection of NXOpen.CAE.Optimization.TBSOptimizationSolution |
TBSOutputControlOptions Class |
Represents the output result control options of the optimization |
TBSRestrictArea Class |
Represents the restrictions for the design variable in an optimization |
TBSRestrictAreaBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSRestrictArea |
TBSRestrictAreaCollection Class |
Represents a collection of NXOpen.CAE.Optimization.TBSRestrictArea |
TBSShapeLinkCondition Class |
Represents the definition of link condition for shape restriction |
TBSShapeOptimizationParameters Class |
Represents the control parameters of shape optimization |
TBSShapeOptimizationSolution Class |
Represents a shape optimization solution |
TBSShapeOptimizationSolutionBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSShapeOptimizationSolution . |
TBSShapeRestrictArea Class |
Represents the restrictions of the design variable in Shape optimization |
TBSShapeRestrictAreaBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSShapeRestrictArea |
TBSSingleObjective Class |
Represents a single objective |
TBSSmooth Class |
Represents the parameters that control the generation of surfaces by optimization |
TBSSmoothBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSSmooth . |
TBSSmoothCollection Class |
Represents a collection of NXOpen.CAE.Optimization.TBSSmooth |
TBSStopCondition Class |
Represents the condtion to end an optimization |
TBSTestFunction Class |
Represents a test displacement for shape optimization or bead optimization |
TBSTopologyControllerOptimizationParameters Class |
Represents the parameters to control an optimization in controller strategy |
TBSTopologyLinkCondition Class |
Represents the definition of symmetry and link conditions for topology optimization |
TBSTopologyOptimizationSolution Class |
Represents the topology optimization solution |
TBSTopologyOptimizationSolutionBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSTopologyOptimizationSolution . |
TBSTopologyRestrictArea Class |
Represents the restrictions of the design variable in topology optimization |
TBSTopologyRestrictAreaBuilder Class |
Represents the builder of NXOpen.CAE.Optimization.TBSTopologyRestrictArea |
TBSTopologySensitivityOptimizationParameters Class |
Represents the parameters to control an optimization in sensitivity strategy |