TBSDesignResponseBuilderResponse Enumeration¶
NXOpen.CAE.Optimization.TBSDesignResponseBuilder.Response is an alias for NXOpen.CAE.Optimization.TBSDesignResponseBuilderResponse
-
class
NXOpen.CAE.Optimization.
TBSDesignResponseBuilderResponse
¶ Bases:
object
Defines the design response type
Enum Members
Enum Member Enum Member Description DynamicFrequency Eigenfrequency from modal analysis DynamicFrequencyKressissel Eigenfrequency calculated with Kreisselmaier-Steinhauser formula Volume Volume of element VolumeFill Volume of element Weight Weight of element DisplacementAbsolute Absolute nodal displacement DisplacementX Nodal displacement in X-direction DisplacementY Nodal displacement in Y-direction DisplacementZ Nodal displacement in Z-direction DisplacementXAbsolute Absolute nodal displacement in X-direction DisplacementYAbsolute Absolute nodal displacement in Y-direction DisplacementZAbsolute Absolute nodal displacement in Z-directionm RotationAbsolute Absolute rotation RotationX Nodal rotation around X-axis RotationY Nodal rotation around Y-axis RotationZ Nodal rotation around Z-axis RotationXAbsolute Absolute nodal rotation around X-axis RotationYAbsolute Absolute nodal rotation around Y-axis RotationZAbsolute Absolute nodal rotation around Z-axis StrainEnergy Strain energy CenterGravityX Center of gravity for the X-direction CenterGravityY Center of gravity for the Y-direction CenterGravityZ Center of gravity for the Z-direction InertiaXx Moment of inertia around X-X-direction InertiaXy Moment of inertia around X-Y-direction InertiaXz Moment of inertia around X-Z-direction InertiaYy Moment of inertia around Y-Y-direction InertiaYz Moment of inertia around Y-Z-direction InertiaZz Moment of inertia around Z-Z-direction ReactionForceAbsolute Absolute nodal reaction force ReactionForceX Nodal reaction force in X-direction ReactionForceY Nodal reaction force in Y-direction ReactionForceZ Nodal reaction force in Z-direction ReactionForceXAbsolute Absolute nodal reaction force in X-direction ReactionForceYAbsolute Absolute nodal reaction force in Y-direction ReactionForceZAbsolute Absolute nodal reaction force in Z-direction ReactionForceRotationAbsolute Absolute nodal reaction moment ReactionForceRotationX Nodal reaction moment around X-axis ReactionForceRotationY Nodal reaction moment around Y-axis ReactionForceRotationZ Nodal reaction moment around Z-axis ReactionForceRotationXAbsolute Absolute nodal reaction moment around X-axis ReactionForceRotationYAbsolute Absolute nodal reaction moment around Y-axis ReactionForceRotationZAbsolute Absolute nodal reaction moment around Z-axis InternalForceAbsolute Absolute nodal internal force InternalForceX Nodal internal force in X-direction InternalForceY Nodal internal force in Y-direction InternalForceZ Nodal internal force in Z-direction InternalForceXAbsolute Absolute nodal internal force in X-direction InternalForceYAbsolute Absolute nodal internal force in Y-direction InternalForceZAbsolute Absolute nodal internal force in Z-direction InternalForceRotationAbsolute Absolute nodal internal moment InternalForceRotationX Nodal internal moment around X-axis InternalForceRotationY Nodal internal moment around Y-axis InternalForceRotationZ Nodal internal moment around Z-axis InternalForceRotationXAbsolute Absolute nodal internal moment around X-axis InternalForceRotationYAbsolute Absolute nodal internal moment around Y-axis InternalForceRotationZAbsolute Absolute nodal internal moment around Z-axis FrequencyResponseAccelerationX Acceleration in X-direction for frequency response FrequencyResponseAccelerationY Acceleration in Y-direction for frequency response FrequencyResponseAccelerationZ Acceleration in Z-direction for frequency response FrequencyResponseCompliance Dynamic compliance for frequency response FrequencyResponseDbaPressure Sound pressure level (dBA) FrequencyResponseDbPressure Sound pressure level (dB) FrequencyResponseDisplacementAbsolute Absolute amplitude for frequency response FrequencyResponseDisplacementXAbsolute Amplitude in X-direction for frequency response FrequencyResponseDisplacementYAbsolute Amplitude in Y-direction for frequency respons FrequencyResponseDisplacementZAbsolute Amplitude in Z-direction for frequency respons FrequencyResponsePhaseXAbsolute Phase in X-direction for frequency response FrequencyResponsePhaseYAbsolute Phase in Y-direction for frequency response FrequencyResponsePhaseZAbsolute Phase in Z-direction for frequency response FrequencyResponsePressure Instantaneous sound pressure FrequencyResponseRmsPressure Effective sound pressure FrequencyResponseVelocityXAbsolute Velocity in X-direction for frequecy response FrequencyResponseVelocityYAbsolute Velocity in Y-direction for frequecy response FrequencyResponseVelocityZAbsolute Velocity in Z-direction for frequecy response FrequencyResponseNvhSolid Surface normal velocity equivalent. Referenced node group, must be on solid elements FrequencyResponseNvhShell Surface normal velocity equivalent. Referenced node group, must be on plate or shell elements MisesStressHypothesis Mises Stress hypothesis MaximumPrincipalStress Maximum principal Stress MinimumAbsolutePrincipalStress Absolute value of the minimum principal Stress MaximumAbsolutePrincipalStress Maximum of absolute value of the principal stress -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-