Hookes Enumeration¶
-
class
NXOpen.CAE.Optimization.
Hookes
¶ Bases:
object
Represents the Hooke’s location
Deprecated since version NX10.0.0: Use the ShellSection property on one of the following classes -
NXOpen.CAE.ResultMeasureResultSectionOptions
,NXOpen.CAE.ResultMeasureResultDirectionSectionOptions
, orNXOpen.CAE.ResultMeasureResultAllOptions
Enum Members
Enum Member Enum Member Description Top Top Bottom Bottom Middle Middle Minimum Minimum Maximum Maximum -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-