ResultMeasureResultAllOptions Class¶
-
class
NXOpen.CAE.
ResultMeasureResultAllOptions
¶ Bases:
NXOpen.CAE.ResultMeasureResultOptions
Represents the combination of all result options for result measure
To obtain an instance of this class use
NXOpen.CAE.ResultMeasureCollection
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
SetAbsoluteValue | Set the option to use absolute values |
SetAddBeamFillets | Set the option to add beam fillets for calculation of beam stresses only |
SetBeamFilletRadius | Set the beam fillet radius if adding beam fillets for calculation of beam results only |
SetBeamSection | Set the beam section for beam stress/strain results |
SetCalculateBeamResults | Set the option to calculate beam stresses for beam results only |
SetCoordinateSystem | Set the coordinate system for directional components |
SetOperation | Set the operation type |
SetPlynum | Set the ply num in result option |
SetShellSection | Set the shell section for shell stress/strain results |
SetUnit | Set the unit |
Method Detail¶
Dispose¶
-
ResultMeasureResultAllOptions.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
SetAddBeamFillets¶
-
ResultMeasureResultAllOptions.
SetAddBeamFillets
¶ Set the option to add beam fillets for calculation of beam stresses only
Signature
SetAddBeamFillets(bAddBeamFillets)
Parameters: bAddBeamFillets (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamFilletRadius¶
-
ResultMeasureResultAllOptions.
SetBeamFilletRadius
¶ Set the beam fillet radius if adding beam fillets for calculation of beam results only
Signature
SetBeamFilletRadius(beamFilletRadius)
Parameters: beamFilletRadius (float) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetBeamSection¶
-
ResultMeasureResultAllOptions.
SetBeamSection
¶ Set the beam section for beam stress/strain results
Signature
SetBeamSection(eBeamSect)
Parameters: eBeamSect ( NXOpen.CAE.ResultSection
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCalculateBeamResults¶
-
ResultMeasureResultAllOptions.
SetCalculateBeamResults
¶ Set the option to calculate beam stresses for beam results only
Signature
SetCalculateBeamResults(bCalcBeamResults)
Parameters: bCalcBeamResults (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCoordinateSystem¶
-
ResultMeasureResultAllOptions.
SetCoordinateSystem
¶ Set the coordinate system for directional components
Signature
SetCoordinateSystem(eCsys)
Parameters: eCsys ( NXOpen.CAE.ResultCoordinateSystem
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetShellSection¶
-
ResultMeasureResultAllOptions.
SetShellSection
¶ Set the shell section for shell stress/strain results
Signature
SetShellSection(eShellSect)
Parameters: eShellSect ( NXOpen.CAE.ResultSection
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)