ResultMeasureResultOptions Class¶
-
class
NXOpen.CAE.
ResultMeasureResultOptions
¶ Bases:
NXOpen.TransientObject
Represents the basic result options for result measure
To obtain an instance of this class use
NXOpen.CAE.ResultMeasureCollection()
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
SetAbsoluteValue | Set the option to use absolute values |
SetOperation | Set the operation type |
SetPlynum | Set the ply num in result option |
SetUnit | Set the unit |
Method Detail¶
Dispose¶
-
ResultMeasureResultOptions.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
SetAbsoluteValue¶
-
ResultMeasureResultOptions.
SetAbsoluteValue
¶ Set the option to use absolute values
Signature
SetAbsoluteValue(bAbsValue)
Parameters: bAbsValue (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetOperation¶
-
ResultMeasureResultOptions.
SetOperation
¶ Set the operation type
Signature
SetOperation(eOperation)
Parameters: eOperation ( NXOpen.CAE.ResultMeasureOperation
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPlynum¶
-
ResultMeasureResultOptions.
SetPlynum
¶ Set the ply num in result option
Signature
SetPlynum(plynum)
Parameters: plynum (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUnit¶
-
ResultMeasureResultOptions.
SetUnit
¶ Set the unit
Signature
SetUnit(tUnit)
Parameters: tUnit ( NXOpen.Unit
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)