ResultMeasureOperation Enumeration¶
NXOpen.CAE.ResultMeasure.Operation is an alias for NXOpen.CAE.ResultMeasureOperation
-
class
NXOpen.CAE.
ResultMeasureOperation
¶ Bases:
object
Operation type
Enum Members
Enum Member Enum Member Description Minimum Evaluate for the minimum value Maximum Evaluate for the maximum value MeanAverage Evaluate for the mean average value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-