ResultMeasureCollection Class¶
-
class
NXOpen.CAE.
ResultMeasureCollection
¶ Bases:
object
Provides methods for managing ResultMeasures
NXOpen.CAE.ResultMeasure
To obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateModelSubset | Create a model subset for result measure |
CreateNewResultOptions | Create a result options for result measure |
CreateResultMeasure | Create a ResultMeasure |
CreateResultMeasureNew | Create a ResultMeasure |
CreateResultOptions | Create a result options for result measure |
CreateResultOptionsNew | Create a result options for result measure |
DeleteMeasures | Delete list of result measures |
Find | Finds the NXOpen.CAE.ResultMeasure with the given identifier as recorded in a journal. |
UpdateMeasures | Update list of result measures. |
Method Detail¶
CreateModelSubset¶
-
ResultMeasureCollection.
CreateModelSubset
¶ Create a model subset for result measure
Signature
CreateModelSubset(eSubset)
Parameters: eSubset ( NXOpen.CAE.ResultMeasureSubsetSelection
) –Returns: Return type: NXOpen.CAE.ResultMeasureModelSubset
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateNewResultOptions¶
-
ResultMeasureCollection.
CreateNewResultOptions
¶ Create a result options for result measure
Signature
CreateNewResultOptions(tSol, tResultReference, tResultLoadcase, tResultIteration, bAllSubiterations, tResultSubIteration, pType, eComp)
Parameters: - tSol (
NXOpen.CAE.SimSolution
) – - tResultReference (
NXOpen.CAE.SimResultReference
) – - tResultLoadcase (
NXOpen.CAE.Loadcase
) – - tResultIteration (
NXOpen.CAE.Iteration
) – - bAllSubiterations (bool) – to be used select all sub iterations
- tResultSubIteration (
NXOpen.CAE.Iteration
) – - pType (
NXOpen.CAE.ResultType_Struct
) – - eComp (
NXOpen.CAE.ResultComponent
) –
Returns: Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- tSol (
CreateResultMeasure¶
-
ResultMeasureCollection.
CreateResultMeasure
¶ Create a ResultMeasure
Signature
CreateResultMeasure(tSol, iStepIndex, iIterIndex, pType, eComp, expName)
Parameters: - tSol (
NXOpen.CAE.SimSolution
) – - iStepIndex (int) –
- iIterIndex (int) –
- pType (
NXOpen.CAE.ResultType_Struct
) – - eComp (
NXOpen.CAE.ResultComponent
) – - expName (str) –
Returns: The created result measure object
Return type: New in version NX8.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.ResultMeasureCollection.CreateResultMeasureNew()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
- tSol (
CreateResultMeasureNew¶
-
ResultMeasureCollection.
CreateResultMeasureNew
¶ Create a ResultMeasure
Signature
CreateResultMeasureNew(pResOpt, pSubset, expName)
Parameters: - pResOpt (
NXOpen.CAE.ResultMeasureResultOptions
) – - pSubset (
NXOpen.CAE.ResultMeasureModelSubset
) – The model subset, can be null - expName (str) – The new expression name for the result measure
Returns: The created result measure object
Return type: New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- pResOpt (
CreateResultOptions¶
-
ResultMeasureCollection.
CreateResultOptions
¶ Create a result options for result measure
Signature
CreateResultOptions(tSol, iStepIndex, iIterIndex, pType, eComp)
Parameters: - tSol (
NXOpen.CAE.SimSolution
) – - iStepIndex (int) –
- iIterIndex (int) –
- pType (
NXOpen.CAE.ResultType_Struct
) – - eComp (
NXOpen.CAE.ResultComponent
) –
Returns: Return type: New in version NX8.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.SimResultReference
:CreateResultMeasureNew()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
- tSol (
CreateResultOptionsNew¶
-
ResultMeasureCollection.
CreateResultOptionsNew
¶ Create a result options for result measure
Signature
CreateResultOptionsNew(tSol, tResultReference, iStepIndex, iIterIndex, pType, eComp)
Parameters: - tSol (
NXOpen.CAE.SimSolution
) – - tResultReference (
NXOpen.CAE.SimResultReference
) – - iStepIndex (int) –
- iIterIndex (int) –
- pType (
NXOpen.CAE.ResultType_Struct
) – - eComp (
NXOpen.CAE.ResultComponent
) –
Returns: Return type: New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.CAE.Iteration
:CreateNewResultOptions()
instead.License requirements: nx_masterfem (“Finite Element Modeling”)
- tSol (
DeleteMeasures¶
-
ResultMeasureCollection.
DeleteMeasures
¶ Delete list of result measures
Signature
DeleteMeasures(objects)
Parameters: objects (list of NXOpen.CAE.ResultMeasure
) – The objects to be updatedNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Find¶
-
ResultMeasureCollection.
Find
¶ Finds the
NXOpen.CAE.ResultMeasure
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the ResultMeasure you want Returns: The found ResultMeasure Return type: NXOpen.CAE.ResultMeasure
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
UpdateMeasures¶
-
ResultMeasureCollection.
UpdateMeasures
¶ Update list of result measures.
Will open each measure’s associated result file, and recompute requested value
Signature
UpdateMeasures(objects)
Parameters: objects (list of NXOpen.CAE.ResultMeasure
) – The objects to be updatedNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)