SimResultReference Class¶
-
class
NXOpen.CAE.
SimResultReference
¶ Bases:
NXOpen.TaggedObject
,NXOpen.CAE.IPostScenarioDataSource
Represents a Result Reference in the .
sim files.
For more information, refer to the Solver language documentation in the SolverLanguageDocumentation.
This class is not created directly by the user.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
CompanionResults | Returns the CAE Companion Results collection belonging to this Result Reference |
Methods¶
Method | Description |
---|---|
GetManagedResultFile | Get the managed result file name |
GetResultFile | Get the result file directory and result file name |
GetResultFileUnits | Get basic 6 units which are stored with solution used for loading the result file |
SetInferredResultFile | Clear previously specified result file location |
SetInferredResultFileUnits | Clears previously specified result file units |
SetLocalResultFile | Specify local result file |
SetManagedResultFile | Specify managed result file |
SetResultFileUnits | Set result file units |
Enumerations¶
SimResultReferenceType Enumeration | Result Types |
CompanionResults¶
-
SimResultReference.
CompanionResults
¶ Returns the CAE Companion Results collection belonging to this Result Reference
Signature
CompanionResults
New in version NX10.0.0.
Returns: Return type: NXOpen.CAE.CompanionResultCollection
Method Detail¶
GetManagedResultFile¶
-
SimResultReference.
GetManagedResultFile
¶ Get the managed result file name
Signature
GetManagedResultFile()
Returns: managed result file name Return type: str New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultFile¶
-
SimResultReference.
GetResultFile
¶ Get the result file directory and result file name
Signature
GetResultFile()
Returns: a tuple Return type: A tuple consisting of (resultfiledir, resfilename) resultfiledir is a str. directly path where result file is stored resfilename is a str. result file name New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResultFileUnits¶
-
SimResultReference.
GetResultFileUnits
¶ Get basic 6 units which are stored with solution used for loading the result file
Signature
GetResultFileUnits()
Returns: 6 basic units used to define the quantities in result file in order of mass, length, time, temperature, angle, and thermal energy Return type: list of NXOpen.Unit
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetInferredResultFile¶
-
SimResultReference.
SetInferredResultFile
¶ Clear previously specified result file location
Signature
SetInferredResultFile()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetInferredResultFileUnits¶
-
SimResultReference.
SetInferredResultFileUnits
¶ Clears previously specified result file units
Signature
SetInferredResultFileUnits()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLocalResultFile¶
-
SimResultReference.
SetLocalResultFile
¶ Specify local result file
Signature
SetLocalResultFile(dirpath, filename)
Parameters: - dirpath (str) – directory name
- filename (str) – file name
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetManagedResultFile¶
-
SimResultReference.
SetManagedResultFile
¶ Specify managed result file
Signature
SetManagedResultFile(file)
Parameters: file (str) – file name New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetResultFileUnits¶
-
SimResultReference.
SetResultFileUnits
¶ Set result file units
Signature
SetResultFileUnits(units)
Parameters: units (list of NXOpen.Unit
) – 6 units for mass, length, time, temperature, angle, and thermal energyNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)