ResultMeasureSubsetSelection Enumeration¶
NXOpen.CAE.ResultMeasure.SubsetSelection is an alias for NXOpen.CAE.ResultMeasureSubsetSelection
-
class
NXOpen.CAE.
ResultMeasureSubsetSelection
¶ Bases:
object
Model subset selection type
Enum Members
Enum Member Enum Member Description NotSet No subset selection, evaluate for entire model Geometry Evaluate for subset selection of geometry entities FiniteElement Evaluate for subset selection of finite element entities -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-