ResultSection Enumeration

NXOpen.CAE.Result.Section is an alias for NXOpen.CAE.ResultSection

class NXOpen.CAE.ResultSection

Bases: object

Result sections

Enum Members

Enum Member Enum Member Description
NotApplicable
Top
Middle
Bottom
Minimum
Maximum
StressRecoveryPointC
StressRecoveryPointD
StressRecoveryPointE
StressRecoveryPointF
All
Bending
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.