ResultCoordinateSystem Enumeration¶
NXOpen.CAE.Result.CoordinateSystem is an alias for NXOpen.CAE.ResultCoordinateSystem
-
class
NXOpen.CAE.
ResultCoordinateSystem
¶ Bases:
object
Coordinate systems
Enum Members
Enum Member Enum Member Description AbsoluteRectangular AbsoluteCylindrical AbsoluteSpherical WorkRectangular WorkCylindrical WorkSpherical Local Material Material coordinate system is applicable only when such coordinate systems are defined in the results model; if no material coordinate system is defined NXOpen.CAE.ResultCoordinateSystem.AbsoluteRectangular
will be usedSelectRectangular SelectCylindrical SelectSpherical -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-