TBSTopologyControllerOptimizationParametersSpeed Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParameters.Speed is an alias for NXOpen.CAE.Optimization.TBSTopologyControllerOptimizationParametersSpeed
-
class
NXOpen.CAE.Optimization.
TBSTopologyControllerOptimizationParametersSpeed
¶ Bases:
object
Specifies the step size of increment
Enum Members
Enum Member Enum Member Description VerySlow Very small stepsize Slow Small stepsize Moderate Moderate stepsize Medium Medium stepsize Fast Fast large step size Iteration Step size is modified dynamically so the optimization end after the given number of iterations -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-